2025-05-30 12:28 AM
Before Ctrl-f used to bring up the Find/Replace dialog, now there is that box at the top instead.
How do I restore the old find as new new one is a bit rubbish...
2025-05-30 1:04 AM - edited 2025-05-30 1:48 AM
Hello @Wood.Andy
It seems that the old Find/Replace dialog box is not available on the last version. I've escalated your point to the concerned team (under internal ticket number 211180), so they review the possibility to reimplemented on the future (without any engagement).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-30 1:06 AM
Thanks!
There was an option on an earlier release to do this from what I remember but it it must have been removed.
I suppose some would call this progress...
2025-05-30 6:07 AM
Search -> File or Ctrl+H will bring up search/replace functionality.
2025-05-30 6:10 AM
Yes that does work but the old Ctrl-f is much more convenient and intuitive especially for multiple replace.
But thanks!
2025-07-25 1:12 AM
They put it back - great!
2026-05-08 12:34 PM
What version of cubeide was it re-implemented?