cancel
Showing results for 
Search instead for 
Did you mean: 

CODE DUMPING ISSUE

sram.1
Associate II

 

STMicroelectronics ST-LINK GDB server. Version 7.3.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.

Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled

Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Encountered Error when opening D:\stmd\STM32CubeIDE_1.12.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.600.202301161003\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit. 

 

I tried uninstalling and reinstalling 2-3 times and i changed the path. but i am getting the same error. Please give me a solution.

1 REPLY 1
Souhaib MAZHOUD
ST Employee

Hi @sram.1 

Thank you for posting!

I advise to try using the last version of STM32CubeIDE 1.13.1, otherwise could you share the name of the board you using.

Thank you

Souhaib