cancel
Showing results for 
Search instead for 
Did you mean: 

Build Analyzer issue

matt-crc
Associate III

Hello,

Is there a trick to get the Build Analyzer to produce data every time the code is compiled?   It seems like the only way I can get it to update the window is if I change something in the linker script file and recompile again.   Is there an easier way or a setting that needs to be set?

thanks

Matthew

 

2 REPLIES 2
Pavel A.
Evangelist III

PavelA_0-1741577029014.png

 

Hi @Pavel A. 

I just tried your suggestion, and when the "auto" is turned on, the refresh button is disabled:

mattcrc_0-1741577862074.png

turning off "Auto" re-enables that button, but I still have the original problem of the build analyzer not updating.

Either the build analyzer window is blank, or it is using data from an older compile.