cancel
Showing results for 
Search instead for 
Did you mean: 

Build Analyzer for MAP file

roshangeoroy
Associate

Build Analyzer output for MAP file includes .bss and other sections that should be in RAM only, in the flash as well. Is this the expected output?

roshangeoroy_0-1743576860756.png

As you can see in the image, .bss and ._user_head_stack is included in the FLASH as well. 

 

1 REPLY 1
Pavel A.
Super User

IMHO this is not the expected output. The flash (load) addresses of bss and stack both are 0x1389c, this means they are zero size. The tool could do better and hide sections of zero size that have non-zero VMA size in other place.