cancel
Showing results for 
Search instead for 
Did you mean: 

.ioc files have blue/green icon on macOS (after 2.0.0 upgrade?)

chriskuku
Senior III

Strange things are happening: I'm running STM32CubeIDE under macOS 15.7.2 (I must admit it is OCLP Sequoia). A couple of minutes ago I was able to open .ioc files in my project - not sure whether that was before the upgrade. Now
the .ioc are upper strip blue, lower half green. What does that mean? 

chriskuku_0-1766226612390.png

When I invoke the .ioc by double click, it switches over to my Windows VM (Parallels) and fires up CubeMX there (a very old version). When the VM is not running, STM32CubeIDE does nothing. The .ioc is not opened like I was used to before. I'm now updating. I'm puzzled.

1 ACCEPTED SOLUTION

Accepted Solutions
Andrew Neil
Super User

The CubeMX functionality was removed from CubeIDE v2.0.0:

STM32CubeIDE 2.0.0 released

So now .ioc files can be opened in CubeMX only - not (directly) in CubeIDE:

STM32CubeIDE 2.0.0 workflow tutorial

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

View solution in original post

3 REPLIES 3
Andrew Neil
Super User

The CubeMX functionality was removed from CubeIDE v2.0.0:

STM32CubeIDE 2.0.0 released

So now .ioc files can be opened in CubeMX only - not (directly) in CubeIDE:

STM32CubeIDE 2.0.0 workflow tutorial

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Scream! Why that? 

Reason & Discussion here:

IDE Version 2.0.0 - why remove MX ?

In particular, this post describes the rationale behind it.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.