2025-03-07 12:57 AM
I need to add the BSP libraries for the STM32H735G-DK board to enable display functionality. I have downloaded the STM32CubeH7 package and navigated to the Driver folder, where I selected my board and found the necessary BSP libraries.
However, when I open STM32CubeIDE, go to Project Properties → C/C++ General, and attempt to add the BSP folder path, the IDE does not recognize the libraries. Instead, I only see the _htmresc file within the folder. Normally, when I open the directory manually, the libraries are present, but they do not appear within the IDE.
Solved! Go to Solution.
2025-03-12 3:05 AM
hi @KDJEM.1 , I use the STM32H735G-DK, but when using the board for createt a project, I don't see the pins.
2025-03-17 4:09 AM
hello @KDJEM.1 , I don't know why, but this library is giving me an error, I’ll attach the project.