cancel
Showing results for 
Search instead for 
Did you mean: 

creating freeRTOS project for STM32F746ZG board in Visual Studio Code environment

Jordalic
Associate II

Hey,

I have STM32F746ZG board and want to start a project using freeRTOS in VisualStudioCode environment.

So far I've used stm32cube extension in VScode and imported the project, but the are lot of variables and functions which are not defined ( bad import I assume).  Also I need to use FreeRTOS rather than cmsisRTOS. How should I approach this if it's possible at all?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0