cancel
Showing results for 
Search instead for 
Did you mean: 

Preserving EEPROM-Emulation area when programming new code - VScode with JLink

ETX
Associate II

I already posted this question on stackexchange, but unfortunately no answers, so please don't me asking here again.

I'm using the last flash page (page 31: 0x0800 F800 - 0x0800 FFFF2) as eeprom emulation area on my STM32G030C8.
I'm working with VScode and programming + debugging the flash with JLink over USB.

Is there a way to prevent the eeprom emulation area from being erased when programming new code, as there is stored some calibration data?

Where or how can I manage erasing only part of the flash, when using normal build and debugging command in VScode?

Thanks!

1 ACCEPTED SOLUTION

Accepted Solutions
ETX
Associate II
Thanks for your feedback.
 
By now I solved my problem this way:
 
(1) Modify the linker script 'STM32G030C8Tx_FLASH.ld' and add the EE emulation area
MEMORY
{
RAM (xrw)      : ORIGIN = 0x20000000, LENGTH = 8K
FLASH (rx)      : ORIGIN = 0x8000000, LENGTH = 62K
EMULATED_EEPROM    (xrw)   : ORIGIN = 0x0800F800,   LENGTH = 2K
}
 
/* Define output sections */
SECTIONS
{
/* The startup code into "FLASH" Rom type memory */
  .ourData :
  {
. = ALIGN(4);
*(.ourData)
. = ALIGN(4);
  } >EMULATED_EEPROM
.
.
.
 
(2) Change linker script name (to e.g. STM32G030C8Tx_EE_FLASH.ld) for MXCube not to erase it when updating code
(3) Modify linker script path in 'CMakeLists.txt' like this
 
# Set linker script
set(linker_script_SRC               ${PROJ_PATH}/STM32G030C8Tx_EE_FLASH.ld)
set(EXECUTABLE                      ${CMAKE_PROJECT_NAME})
 
I've been reading out the memory areas and it seems to work fine.
If there is anything wrong or to improve, please give some feedback.
Thanks.

View solution in original post

2 REPLIES 2
Pavel A.
Super User

Does the J-Link (J-Flash) do full erase? Is this what it says in its log?

Just ensure that your program file (elf or hex) does not contain code or data in these flash sectors and they should not be erased when programming.

 

ETX
Associate II
Thanks for your feedback.
 
By now I solved my problem this way:
 
(1) Modify the linker script 'STM32G030C8Tx_FLASH.ld' and add the EE emulation area
MEMORY
{
RAM (xrw)      : ORIGIN = 0x20000000, LENGTH = 8K
FLASH (rx)      : ORIGIN = 0x8000000, LENGTH = 62K
EMULATED_EEPROM    (xrw)   : ORIGIN = 0x0800F800,   LENGTH = 2K
}
 
/* Define output sections */
SECTIONS
{
/* The startup code into "FLASH" Rom type memory */
  .ourData :
  {
. = ALIGN(4);
*(.ourData)
. = ALIGN(4);
  } >EMULATED_EEPROM
.
.
.
 
(2) Change linker script name (to e.g. STM32G030C8Tx_EE_FLASH.ld) for MXCube not to erase it when updating code
(3) Modify linker script path in 'CMakeLists.txt' like this
 
# Set linker script
set(linker_script_SRC               ${PROJ_PATH}/STM32G030C8Tx_EE_FLASH.ld)
set(EXECUTABLE                      ${CMAKE_PROJECT_NAME})
 
I've been reading out the memory areas and it seems to work fine.
If there is anything wrong or to improve, please give some feedback.
Thanks.