cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP257f-dk OpenAMP No such file or directory

Nicolas_D
Associate

Hello,

I am encountering an issue when enabling the OpenAMP middleware in CubeMX for a new project targeting the STM32MP257F‑DK board. After creating the project and activating only the OpenAMP middleware (see attached screenshot), the build fails because several required files are missing. Below is the full error message generated during compilation.

Thank you in advance for your help.

Nicolas_D_0-1742898217765.png

Nicolas_D_0-1742898354428.png

 

11:12:24 **** Build of configuration Debug for project openAMP_mp257_CM33 ****

make -j12 all

arm-none-eabi-gcc "../OPENAMP/mbox_ipcc.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DCORE_CM33 -DUSE_HAL_DRIVER -DSTM32MP257Fxx -DNO_ATOMIC_64_SUPPORT -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DVIRTIO_SLAVE_ONLY -c -I../Core/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc/Legacy -I../../Drivers/CMSIS/Device/ST/STM32MP2xx/Include -I../../Drivers/CMSIS/Include -I../OPENAMP -I../../Middlewares/Third_Party/OpenAMP/virtual_driver -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"OPENAMP/mbox_ipcc.d" -MT"OPENAMP/mbox_ipcc.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "OPENAMP/mbox_ipcc.o"

arm-none-eabi-gcc "../OPENAMP/open_amp.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DCORE_CM33 -DUSE_HAL_DRIVER -DSTM32MP257Fxx -DNO_ATOMIC_64_SUPPORT -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DVIRTIO_SLAVE_ONLY -c -I../Core/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc/Legacy -I../../Drivers/CMSIS/Device/ST/STM32MP2xx/Include -I../../Drivers/CMSIS/Include -I../OPENAMP -I../../Middlewares/Third_Party/OpenAMP/virtual_driver -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"OPENAMP/open_amp.d" -MT"OPENAMP/open_amp.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "OPENAMP/open_amp.o"

arm-none-eabi-gcc "../OPENAMP/openamp_log.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DCORE_CM33 -DUSE_HAL_DRIVER -DSTM32MP257Fxx -DNO_ATOMIC_64_SUPPORT -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DVIRTIO_SLAVE_ONLY -c -I../Core/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc/Legacy -I../../Drivers/CMSIS/Device/ST/STM32MP2xx/Include -I../../Drivers/CMSIS/Include -I../OPENAMP -I../../Middlewares/Third_Party/OpenAMP/virtual_driver -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"OPENAMP/openamp_log.d" -MT"OPENAMP/openamp_log.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "OPENAMP/openamp_log.o"

arm-none-eabi-gcc "../OPENAMP/rsc_table.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DCORE_CM33 -DUSE_HAL_DRIVER -DSTM32MP257Fxx -DNO_ATOMIC_64_SUPPORT -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DVIRTIO_SLAVE_ONLY -c -I../Core/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc/Legacy -I../../Drivers/CMSIS/Device/ST/STM32MP2xx/Include -I../../Drivers/CMSIS/Include -I../OPENAMP -I../../Middlewares/Third_Party/OpenAMP/virtual_driver -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"OPENAMP/rsc_table.d" -MT"OPENAMP/rsc_table.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "OPENAMP/rsc_table.o"

../OPENAMP/mbox_ipcc.c:36:1: warning: "/*" within comment [-Wcomment]

arm-none-eabi-gcc "C:/Users/dn/STM32CubeIDE/workspace_1.18.0/openAMP_mp257/Middlewares/Third_Party/OpenAMP/libmetal/lib/system/generic/condition.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DCORE_CM33 -DUSE_HAL_DRIVER -DSTM32MP257Fxx -DNO_ATOMIC_64_SUPPORT -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DVIRTIO_SLAVE_ONLY -c -I../Core/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc/Legacy -I../../Drivers/CMSIS/Device/ST/STM32MP2xx/Include -I../../Drivers/CMSIS/Include -I../OPENAMP -I../../Middlewares/Third_Party/OpenAMP/virtual_driver -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Middlewares/Third_Party/OpenAMP/condition.d" -MT"Middlewares/Third_Party/OpenAMP/condition.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Middlewares/Third_Party/OpenAMP/condition.o"

36 | /* Includes ------------------------------------------------------------------*/

|

In file included from ../OPENAMP/mbox_ipcc.c:37:

../OPENAMP/openamp.h:25:10: fatal error: openamp/open_amp.h: No such file or directory

25 | #include "openamp/open_amp.h"

| ^~~~~~~~~~~~~~~~~~~~

compilation terminated.

make: *** [OPENAMP/subdir.mk:28: OPENAMP/mbox_ipcc.o] Error 1

make: *** Waiting for unfinished jobs....

In file included from ../OPENAMP/open_amp.c:21:

../OPENAMP/openamp.h:25:10: fatal error: openamp/open_amp.h: No such file or directory

25 | #include "openamp/open_amp.h"

| ^~~~~~~~~~~~~~~~~~~~

compilation terminated.

make: *** [OPENAMP/subdir.mk:28: OPENAMP/open_amp.o] Error 1

In file included from ../OPENAMP/rsc_table.h:23,

from ../OPENAMP/rsc_table.c:40:

../OPENAMP/openamp.h:25:10: fatal error: openamp/open_amp.h: No such file or directory

25 | #include "openamp/open_amp.h"

| ^~~~~~~~~~~~~~~~~~~~

compilation terminated.

make: *** [OPENAMP/subdir.mk:28: OPENAMP/rsc_table.o] Error 1

C:/Users/dnrfag/STM32CubeIDE/workspace_1.18.0/openAMP_mp257/Middlewares/Third_Party/OpenAMP/libmetal/lib/system/generic/condition.c:12:10: fatal error: metal/condition.h: No such file or directory

12 | #include <metal/condition.h>

| ^~~~~~~~~~~~~~~~~~~

compilation terminated.

make: *** [Middlewares/Third_Party/OpenAMP/subdir.mk:88: Middlewares/Third_Party/OpenAMP/condition.o] Error 1

"make -j12 all" terminated with exit code 2. Build might be incomplete.

 

11:12:26 Build Failed. 9 errors, 1 warnings. (took 2s.312ms)





1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @Nicolas_D ,

Thanks for your post. This is a known problem we are working on. BZ197530

We hope to provide fix in coming CubeMX release.

In the meantime you might take exemple on OpenAMP application exemple provided in CubeFirmware package and bring it in your project

Olivier 

 

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.