2025-03-12 1:10 AM
Hello,
I'm working on uploading test firmware to the M33 core on the STM32MP257F-EV1 using STM32CubeIDE.
After enabling the OpenAMP function in the .ioc file, I noticed an issue with the files automatically generated under the Middlewares/Third_Party/OpenAMP/ directory: certain placeholders (such as @PROJECT_SYSTEM@) are not being replaced with the correct values. Is there a plan to address this in future updates, or is there a recommended workaround for now?
Thank you.