cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.15.1 released

Semer CHERNI
ST Employee

STM32CubeIDE 1.15.1 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.11.1 that is available for download.

Main issues fixed in this patch:

  • Ticket 177978 : Fixed an issue with ST-LINK firmware upgrade concerning the boards with DFU v2 or older in the version 3.14.5 of ST-LINK GDB server.
  • Ticket 178127 : Fixed an issue with the build settings: The build settings do not save the latest linker modified by the user and select the default linker instead.

Check the errata under this link for more details.

Where do I obtain STM32CubeIDE 1.15.1?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 REPLIES 3
Uwe Bonnes
Principal III

The download page still only offers 1.15.0.

Hey Uwe,

It'll probably take more than 56 minutes...

 

"Always be yourself. Unless you can be a pirateThen always be a pirate.”

...seems so.

AScha3_0-1714044305729.png

 

If you feel a post has answered your question, please click "Accept as Solution".