2024-11-11 12:12 AM - edited 2024-11-11 1:29 AM
I want to place my signing keys in secure location, like HSM or softhsm. Keys get placed but the given arguments dont work for signing through the secure keys within object store of PKCS11.
- If I provide my slot, it givees se3gmentation fault
ept@de3:~/build/senec/yocto$ sudo /home/ept/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32MP_SigningTool_CLI --module /usr/lib/softhsm/libsofthsm2.so -ki 1 -si 5407DACB907 -bin build/tmp/deploy/images/stm32mp1-ems-c2-faa1/arm-trusted-firmware/bl2/tf-a-stm32mp157f-ems-c2-faa1-mx-usb.bin -o tf-a-stm32mp157f-ems-c2-faa1-mx-usb_Signed.stm32 -pwd epteck -type fsbl -la 0x2ffc2500 -ep 0x2ffe9000
-------------------------------------------------------------------
STM32MP Signing Tool v2.15.0
-------------------------------------------------------------------
Error: Invalid slot index valueept@de3:~/build/senec/yocto$
ept@de3:~/build/senec/yocto$ sudo /home/ept/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32MP_SigningTool_CLI --module /usr/lib/softhsm/libsofthsm2.so -ki 1 -si 1409800907 -bin build/tmp/deploy/images/stm32mp1-ems-c2-faa1/arm-trusted-firmware/bl2/tf-a-stm32mp157f-ems-c2-faa1-mx-usb.bin -o tf-a-stm32mp157f-ems-c2-faa1-mx-usb_Signed.stm32 -pwd epteck -type fsbl -la 0x2ffc2500 -ep 0x2ffe9000
-------------------------------------------------------------------
STM32MP Signing Tool v2.15.0
-------------------------------------------------------------------
+++ PKCS#11 interface +++
Library Info:
Manufacturer ID : SoftHSM
Library Description: Implementation of PKCS11
Library Version : 2.5
CryptoKi Version : 2.40
Slots number : 2
Segmentation fault
- If I use slot index to be zero, it says object handled isnt done correctly, same error if we place key or not
ept@de3:~/build/senec/yocto$ sudo /home/ept/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32MP_SigningTool_CLI --module /usr/lib/softhsm/libsofthsm2.so -ki 0x64 -si 0 -bin build/tmp/deploy/images/stm32mp1-ems-c2-faa1/arm-trusted-firmware/bl2/tf-a-stm32mp157f-ems-c2-faa1-mx-usb.bin -o tf-a-stm32mp157f-ems-c2-faa1-mx-usb_Signed.stm32 -pwd epteck -type fsbl -la 0x2ffc2500 -ep 0x2ffe9000 -iv 1
-------------------------------------------------------------------
STM32MP Signing Tool v2.15.0
-------------------------------------------------------------------
+++ PKCS#11 interface +++
Library Info:
Manufacturer ID : SoftHSM
Library Description: Implementation of PKCS11
Library Version : 2.5
CryptoKi Version : 2.40
Slots number : 2
Slot Info:
Slot index : 0
Manufacturer ID : SoftHSM project
Description : SoftHSM slot ID 0x5407dacb
Hardware version : 2.5
Firmware version : 2.5
Token Info:
Manufacturer ID : SoftHSM project
Label : tfa token
Model : SoftHSM v2
Serial number : c2533329d407dacb
PIN min lenght : 4
PIN max lenght : 255
Hardware version : 2.5
Firmware version : 2.5
Public key search object :
ID : 0x64
Error: CKR_OBJECT_HANDLE_INVALID
Error: Cannot extract public key from pkcs11 module !
Question:
- Am I using any argment wrong?
- What am I supposed to put in key-index argument? I have tried with 1 and also with object id of the placed keys
- Will this -pwd argument serve as the SO/user pin for accessing secure keys?
Following: https://wiki.st.com/stm32mpu/wiki/Signing_tool#Additional_PKCS-2311_commands
#STM32MP_SigningTool
2024-11-18 7:06 AM
Hello @saman_,
Could you try testing with STM32CubeProgrammer v2.17 and get back to us with the results ?
Thanks in advance,
Aziz
2024-11-19 11:30 AM
It's the same with both cases:
ept@de3:~/build/senec/yocto$ sudo /home/ept/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32MP_SigningTool_CLI --module /usr/lib/softhsm/libsofthsm2.so -ki 1 -si 1409800907 -bin build/tmp/deploy/images/stm32mp1-ems-c2-faa1/arm-trusted-firmware/bl2/tf-a-stm32mp157f-ems-c2-faa1-mx-usb.bin -o tf-a-stm32mp157f-ems-c2-faa1-mx-usb_Signed.stm32 -pwd epteck -type fsbl -la 0x2ffc2500 -ep 0x2ffe9000
-------------------------------------------------------------------
STM32MP Signing Tool v2.17.0
-------------------------------------------------------------------
+++ PKCS#11 interface +++
Library Info:
Manufacturer ID : SoftHSM
Library Description: Implementation of PKCS11
Library Version : 2.5
CryptoKi Version : 2.40
Slots number : 2
Segmentation fault
2024-12-05 4:58 AM
Hello @saman_ ,
Sorry for the late reply, missed your comment initially.
Your observation is correct since Signing Tool for now takes in the slot offset (Not the identifier). A change request is submitted internally under Ticket 196625 and will be available in STM32CubeProgrammer v2.19.
For now, you can put in the offset after -si option. For example, if it's the first slot you created, the full command should look like this :
STM32MP_SigningTool_CLI --module /usr/lib/softhsm/libsofthsm2.so -ki 1 -si 1 -bin build/tmp/deploy/images/stm32mp1-ems-c2-faa1/arm-trusted-firmware/bl2/tf-a-stm32mp157f-ems-c2-faa1-mx-usb.bin -o tf-a-stm32mp157f-ems-c2-faa1-mx-usb_Signed.stm32 -pwd epteck -type fsbl -la 0x2ffc2500 -ep 0x2ffe9000
Hope this helps,
Aziz