cancel
Showing results for 
Search instead for 
Did you mean: 

qt programing and stm32mp157d-dk1

Sharan
Senior II

hi

i am using stm32mp157d-dk1 and i have downloaded qt creator and i have created a simple hello world window now how to display it in the stm32mp157d-dk1?

 

how to set up cross compilation in order to deploy Qt projects directly from a host Linux machine to the embedded target using qtcreator.

34 REPLIES 34
Sharan
Senior II

i have installed the distribution package and followed the bellow steps

and what do do now to set up qt creator?

6.1.3.2. Install X-LINUX-QT Distribution Package

To install the X-LINUX-QT Distribution Package

  • Clone the meta-st-x-linux-qt git repository
 cd <Distribution Package installation directory>
 git clone -b v1.0.0 https://github.com/STMicroelectronics/meta-st-x-linux-qt.git layers/meta-st/meta-st-x-linux-qt
  • Clone the meta-qt5 git repository
 git clone -b scarthgap https://github.com/meta-qt5/meta-qt5.git layers/meta-qt5
  • For a new environment

Source the build environment with the correct board and layers:

 DISTRO=openstlinux-weston MACHINE=stm32mp2 BSP_DEPENDENCY="layers/meta-qt5 layers/meta-st/meta-st-x-linux-qt" source layers/meta-st/scripts/envsetup.sh
  • For an already installed environment

Add the layers to the Yocto environment:

 cd <Distribution Package installation directory>
 source layers/meta-st/scripts/envsetup.sh
 bitbake-layers add-layer ../layers/meta-qt5 ../layers/meta-st/meta-st-x-linux-qt

and 

I went with developer package as i was not able to do the distribution package

so the steps i followed for developer package was

i downloaded the MP1-DEV-x86 from st website

For x86_64 host architecture i Uncompressed the tarball file to get the SDK installation script. and Ran the SDK installation script. 

for x-linux-qt developer package i downloded the below file(but my board is stm32mp157d-dk1)

Sharan_0-1728889673344.png

i followed these steps

Sharan_1-1728889819073.png

 

 

in the terminal i download qt creator using sudo apt install qtcreator and it installed  (qt 5.15.13) and u had said Qt Creator will be configured automatically and you will get your MPU kit all set in Qt creator. but i cant find anything other than Qt 5.15.13(system)

 

Screenshot from 2024-10-14 12-42-44.png

 

 


Screenshot from 2024-10-14 11-43-45.png

The full MP1 X-LINUX-Qt support will be available in the coming weeks.

Distribution Package allows anyway user to compile with Qt libraries and run Qt application on MP1.

But for Qt creator MP1 kit configuration, you have to do it manually.  Please refer to that post:

https://community.st.com/t5/stm32-mpus-embedded-software-and/qt-creater-setup-for-stm32mp1/m-p/706440

 

For MP2, the SDK-add on configures Qt creator kit automatically, but for MP1, the SDK-Addon is not yet delivered. Sorry of the inconvinience. It will be release soon.

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

i am doing it manually it is showing no compiler can produce code for this  qt version

Screenshot from 2024-10-14 11-43-45.png

Please look at the post I listed before, it will describe how to get the SDK and how to use it

(bitbake st-image-qt -c populate_sdk, ...)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

it is showing like this when i run that

WARNING: Setscene task (/home/sharan/STM32MPU/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/meta/recipes-core/glibc/glibc_2.37.bb:do_populate_sysroot_setscene) failed with exit code '1' - real task will be run instead
NOTE: Tasks Summary: Attempted 496 tasks of which 494 didn't need to be rerun and 2 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 5 seconds

Summary: 2 tasks failed:
/home/sharan/STM32MPU/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/meta/recipes-kernel/linux-libc-headers/linux-libc-headers_6.1.bb:do_unpack
/home/sharan/STM32MPU/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/layers/openembedded-core/meta/recipes-kernel/linux-libc-headers/linux-libc-headers_6.1.bb:do_prepare_recipe_sysroot
Summary: There were 302 ERROR messages, returning a non-zero exit code.

Sharan
Senior II

can someone please verify these steps please check the steps  and correct me if i am wrong                                                                    

steps to download distribution package

1.cd <working directory path>/Distribution-Package

2.repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-6.1-yocto-mickledore-mpu-v24.06.26

3.repo sync

4. DISTRO=openstlinux-weston MACHINE=<machine> source layers/meta-st/scripts/envsetup.s

5.bitbake st-image-weston

Install X-LINUX-QT Distribution Package

6. cd <Distribution Package installation directory>
7.git clone -b v1.0.0 https://github.com/STMicroelectronics/meta-st-x-linux-qt.git layers/meta-st/meta-st-x-linux-qt

8. git clone -b scarthgap https://github.com/meta-qt5/meta-qt5.git layers/meta-qt5

9. DISTRO=openstlinux-weston MACHINE=stm32mp2 BSP_DEPENDENCY="layers/meta-qt5 layers/meta-st/meta-st-x-linux-qt" source layers/meta-st/scripts/envsetup.sh

10.bitbake st-image-qt

11.bitbake st-image-qt -c populate_sdk

12.sdk generation refering to this doc https://wiki.st.com/stm32mpu/wiki/How_to_create_an_SDK_for_OpenSTLinux_distribution and using this command

bitbake -c populate_sdk st-image-weston

Hi Sharan,

  • "For an already installed environment", you have to add new layers by a "bitbale-layer add-layer" command
  • For mp15 DK board, use MACHINE=stm32mp15-disco. This will be simpler.

So you should get these command sequence

4. DISTRO=openstlinux-weston MACHINE=stm32mp15-disco source layers/meta-st/scripts/envsetup.sh

7. git clone -b v1.0.0 https://github.com/STMicroelectronics/meta-st-x-linux-qt.git layers/meta-st/meta-st-x-linux-qt

8. git clone -b scarthgap https://github.com/meta-qt5/meta-qt5.git layers/meta-qt5

9.

bitbake-layers add-layer ../layers/meta-qt5 ../layers/meta-st/meta-st-x-linux-qt

9. DISTRO=openstlinux-weston MACHINE=stm32mp2 BSP_DEPENDENCY="layers/meta-qt5 layers/meta-st/meta-st-x-linux-qt" source layers/meta-st/scripts/envsetup.sh

10.bitbake st-image-qt

11.bitbake st-image-qt -c populate_sdk

 

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Sharan
Senior II

1)first question

after the 5th (that is bitbake st-image-weston) step do u have to execute this commad bitbake st-image-weston -c populate_sdk

2)second question

after the 11th step do we have to execute the bellow one ?

Then install the SDK: execute "xxx.sh" script available in: build-openstlinuxweston-stm32mp15-disco/tmp-glibc/deploy/sdk

3)third question 

how many gb should i need to allocate for the above commands in virtual box and what version of qt creator should i need to install 

4)does the above commands require internet?

"bitbake st-image-weston -c populate_sdk" command is necessary to generate the SDK .sh script.

This SDK .sh script (in build-openstlinuxweston-stm32mp15-disco/tmp-glibc/deploy/sdk) has to be executed.

This will create a SDK directory you will have to refer to in Qt creator.

Qt Creator 12.x.y can be used.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.