Skip to main content
SLetter
Associate III
August 19, 2022
Question

I used STM32CubeMX version 6.3.0 thinking it was the correct version for Ecosystem 3.0 just to discover I should have used STM32CubeMX version 6.2.1. Is there a way to move my projects backwards?

  • August 19, 2022
  • 2 replies
  • 1347 views

I have several projects already configured for STM32MP157C and I don't want to have to build them all over again if I can help it. Also, my team is asking I not move the Ecosystem (but if that is my only answer I will.)

This topic has been closed for replies.

2 replies

debugging
Lead
September 3, 2023

Great question, same here, How do you (re)generate  device tree for an old ECO when Cube MX/IDE/Programmer etc.. tools moved on to newer versions,

Issamos
Super User
September 3, 2023

Hello @SLetter 

You can open .ioc file generated by CubeMX 6.3.0 with CubeMX 6.2.1 . But you have to take a look on the major changes between the two versions and do necessary modifications (I don't think there is a lot of them).

Hope this is helpful. If your question is answered please check this answer as best answer to be diffused.

Best regards

II