2021-04-27 11:34 AM
I am able to build my STM32MP1 Linux project. Below you can see what is built:
I have been trying to follow the guide on the STM32 wiki here: https://wiki.st.com/stm32mpu/wiki/How_to_manage_OpenSTLinux_project_in_STM32CubeIDE#Linux_project
The issue is that there is information that is completely missing from the getting started guide is that when I try to do this step: Run As->STM32 Cortex-A Linux Deployment I get the following screen. Right away this is different from the guide and has an error message that says: Connection "" not available at the top.
Other guides on the wiki mention that the Target Status should be online. Mine is stuck offline and I don't see any indication on how to set that up either.
I currently have 3 USB connections to the STM32MP1 Discovery board. One USB C to a power supply, One USB C, and a micro USB to my PC.
2021-04-29 06:33 AM
Hi @VWied.1 ,
I noticed your same problematics is being addressed in another post :
Please avoid duplicate question at different place.
Olivier