2024-10-21 2:55 AM
Cubeide 1.13 and CubeMX 6.9 can generate the valid code for stm32mp157,but Cubeide 1.14 and CubeMX 6.10 can not! is there a bug or the CubeMX 6.10 have some change for stm32mp157?. MCU Package 1.6.0 and the STMH7xx doesn`t affect it.
void MX_QUADSPI_Init(void)
{
/* USER CODE BEGIN QUADSPI_Init 0 */
/* USER CODE END QUADSPI_Init 0 */
/* USER CODE BEGIN QUADSPI_Init 1 */
/* USER CODE END QUADSPI_Init 1 */
/* USER CODE BEGIN QUADSPI_Init 2 */
/* USER CODE END QUADSPI_Init 2 */
}
why?
2024-10-22 2:13 AM
Hello @nhappy ,
First let me thank you for posting and welcome to the ST Community.
For more investigation, I suggest that you provide your Ioc.File.
Thanks.
Mahmoud
2024-10-22 4:27 AM
Hello @nhappy ,
The issue is confirmed, and it will be investigated by the STM32cubeMX team (Internal ticket number: 194608),
Thanks.
Mahmoud