cancel
Showing results for 
Search instead for 
Did you mean: 

We are using the STM32MP157A device in our application. inter process communication between the both A7 processor with the bare metal programming .

srikanth
Associate III

We are using the STM32MP157A device in our application. inter process communication between the both A7 processor with the bare metal programming we have doubt that how to select the both the cores independently . That is both the A7 processors. We referred the Reference manual .But we unable to get exactly.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
PatrickF
ST Employee

Hi,

using Cortex-A7 SMP in bare-metal is probably a not so easy task.

I guess inter-processor communication within same cluster (i.e the 2 x Cortex-A7 in STM32MP15x) does not need specific HW outside what ARM provides natively.

The IPCC in the STM32MP15x is used for communication between Linux and Cortex-M4, but not within the cluster of the two Cortex-A7.

I think Linux kernel is probably using only shared memory (usually cached DDR), SEV/WFE instructions and GIC SGI interrupts.

Maybe it exist 3rd party company which provide bare-metal libraries or support for that.

ST does not provide any SW nor support for bare-metal on STM32MP15.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NEW ! Sidekick STM32 AI agent, see here

classical spin-locks and memory areas can help you?

For targeting interrupts GIC hardware provide CPU MASK parameters in some software and hardware interrupts.