cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to install AI packages

JYune
Associate II

Reference: https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_OpenSTLinux_Expansion_Package#Configure_the_AI_OpenSTLinux_package_repository

Note that I am still using v2.0.0.

I used to be able to do the following execution on my board, but it is not working anymore. Something has changed.

Board $> wget http://extra.packages.openstlinux.st.com/AI/2.0/pool/config/a/apt-openstlinux-ai/apt-openstlinux-ai_1.0_armhf.deb
Board $> dpkg -i apt-openstlinux-ai_1.0_armhf.deb

The error message is as follows:

root@stm32mp1:~/Downloads# dpkg --install apt-openstlinux-ai_1.0_armhf.deb 
Selecting previously unselected package apt-openstlinux-ai.
(Reading database ... 14442 files and directories currently installed.)
Preparing to unpack apt-openstlinux-ai_1.0_armhf.deb ...
Unpacking apt-openstlinux-ai (1.0) ...
dpkg: dependency problems prevent configuration of apt-openstlinux-ai:
 apt-openstlinux-ai depends on apt-openstlinux (>= 2.1-r0); however:
  Version of apt-openstlinux on system is 1.0-r0.
 
dpkg: error processing package apt-openstlinux-ai (--install):
 dependency problems - leaving unconfigured
Errors were encountered while processing:
 apt-openstlinux-ai

It seems to me that the required apt-openstlinux version for the AI package for v2.0.0 is also updated to v2.1. This needs to be fixed for those who are still using v2.0.0.

2 REPLIES 2
VABRI
ST Employee

@JYune​ 

Thanks for reporting the issue.

It should be fixed now.

BR

Vincent


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Thanks a lot for the update. Much appreciated!