2022-02-25 08:27 AM
Are there any plans to support the STM32MP157F-DK2 board in mainline (vanilla) U-Boot?
It's supported in the ST fork from U-Boot, but with an older version from U-Boot from the year 2020.
Could also ask this in the U-Boot mailing list.
2022-03-10 08:02 AM
Hello @krjdev ,
The support of the mainline U-Boot is not planned for the moment.
I will come back to you if I have more information.
Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'