2024-08-07 4:38 AM
I'm trying to run my application compiled and linked for DDR on STM32MP135F-DK.
Following the wiki istruction it's necessary preliminary to run the DDRInit project on SYSRAM that initialize the DDR and then execute my custom program.
When I execute the DDRInit project the DDR configuration seems to be ok but when ddr_test_data_bus() is executed it fail at the first DDR base address 0xC0000000.
Can someone explain to me why?
Thanks in advance.
Solved! Go to Solution.
2024-08-09 2:24 AM
Hello Olivier.
Thanks for your time but I have understand my mistake.
I'm trying to run the DDRInt project finded inside the STM32MP13XX_CUSTOM_HW folder but using a DK board instead to use the same project on STM32MP135C-DK folder.
Now I have checked and is all working as is!
Thanks for your support.
2024-08-09 2:15 AM
Hi @Sxx ,
Can you please confirm you are using our latest delivery V1.1.0 ?
The provided DDR_Init is supposed to work as is.
Can you maybe further describe how you proceed?
Using Engi boot or booting from SD ?
Thanks
Olivier
2024-08-09 2:24 AM
Hello Olivier.
Thanks for your time but I have understand my mistake.
I'm trying to run the DDRInt project finded inside the STM32MP13XX_CUSTOM_HW folder but using a DK board instead to use the same project on STM32MP135C-DK folder.
Now I have checked and is all working as is!
Thanks for your support.
2024-08-09 4:47 AM
Hi @Sxx
Good to hear, Thanks for feedback !
Olivier