cancel
Showing results for 
Search instead for 
Did you mean: 

stm32mp135 - pcm5102a - sai1a

MWoło.2
Senior III

Hello,

I try to connect a popular Arduino board PCM5102a with my board which is base on STM32MP135.

MWoo2_0-1688975337399.jpeg

I read some documentation from the link

but pcm, i2s and sound topics are something I have only a base knowledge of, so please give some advice and hints.

My dts looks like

 

/ {
    sound {
        compatible = "audio-graph-card";
        label = "STM32MP1-audio-test-card";
		routing =
			"Playback" , "MCLK",
			"Capture" , "MCLK",
			"MICL" , "Mic Bias";
		dais = <&i2s1_port>;
        status = "okay";
    };

    codec: pcm5102a-codec {
        compatible = "ti,pcm5102a";
        #sound-dai-cells = <0>;
        clocks = <&i2s1>;     /* The codec is a consumer of I2S2 master clock */
        clock-names = "MCLK"; /* Feed MCLK codec clock with I2S2 master clock provider */

        codec_port: port {
            codec_endpoint: endpoint {
                remote-endpoint = <&i2s1_endpoint>;
				frame-master;    /* Set codec as master of SAI1A for FS clock. */
				bitclock-master; /* Set codec as master of SAI1A for SCK clock. */
            };
        };
    };
};

	sai1a_pins_mx: sai1a_mx-0 {
		pins {
			pinmux = <STM32_PINMUX('C', 0, AF2)>, /* SAI1_SCK_A */
					 <STM32_PINMUX('C', 3, AF10)>, /* SAI1_MCLK_A */
					 <STM32_PINMUX('E', 11, AF6)>, /* SAI1_FS_A */
					 <STM32_PINMUX('F', 12, AF6)>; /* SAI1_SD_A */
			bias-disable;
			drive-push-pull;
			slew-rate = <0>;
		};
	};

	sai1a_sleep_pins_mx: sai1a_sleep_mx-0 {
		pins {
			pinmux = <STM32_PINMUX('C', 0, ANALOG)>, /* SAI1_SCK_A */
					 <STM32_PINMUX('C', 3, ANALOG)>, /* SAI1_MCLK_A */
					 <STM32_PINMUX('E', 11, ANALOG)>, /* SAI1_FS_A */
					 <STM32_PINMUX('F', 12, ANALOG)>; /* SAI1_SD_A */
		};
	};

&sai1{
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&sai1a_pins_mx>;
	pinctrl-1 = <&sai1a_sleep_pins_mx>;
	status = "okay";

	/* USER CODE BEGIN sai1 */
    #clock-cells = <0>;
    clocks = <&rcc SAI1>, <&scmi_clk CK_SCMI_PLL3_Q>, <&scmi_clk CK_SCMI_PLL3_R>;
    clock-names = "pclk", "x8k", "x11k";
    #sound-dai-cells = <1>;
	/* USER CODE END sai1 */

	sai1a:audio-controller@4400a004{
		status = "okay";

		/* USER CODE BEGIN sai1a */
		compatible = "st,stm32-sai-sub-a";
		reg = <0x4 0x1C>;
		clocks = <&rcc SAI1>;
		clock-names = "sai_ck";
		#clock-cells = <0>;
		dma-names = "tx";
		/*dmas = <&dmamux1 1 87 0x400 0x0>;*/
		/*dma-names = "tx";*/
		i2s1_port: port {
			i2s1_endpoint: endpoint {
				remote-endpoint = <&codec_endpoint>;
				format = "i2s";
				mclk-fs = <256>;
			};
		};
		/* USER CODE END sai1a */
	};
};

 

 I get an error like

 

root@mp1-sagittarius:~# dmesg | grep audio
[    0.057703] OF: /pcm5102a-codec: could not get #clock-cells for /soc/audio-controller@44004000
[   35.535330] platform 4400a004.audio-controller: Fixing up cyclic dependency with pcm5102a-codec
[   39.684607] OF: /pcm5102a-codec: could not get #clock-cells for /soc/audio-controller@44004000
[   39.692414] st,stm32-sai-sub 4400a004.audio-controller: Missing dma channel for stream: 0
[   39.836205] st,stm32-sai-sub 4400a004.audio-controller: ASoC: error at snd_soc_pcm_component_new on 4400a004.audio-controller: -22
[   39.923241] asoc-audio-graph-card sound: ASoC: can't create pcm 4400a004.audio-controller-pcm5102a-hifi :-22
[   39.932041] asoc-audio-graph-card sound: parse error -22
[   40.049044] asoc-audio-graph-card: probe of sound failed with error -22
root@mp1-sagittarius:~# 

 

in optte dts I use CLK_SAI1_PLL4Q for SAI1a.

BR Michal

 

 

11 REPLIES 11

I think I found a links with information, I try and give feedback

https://wiki.st.com/stm32mpu/wiki/How_to_play_audio

https://wiki.st.com/stm32mpu/wiki/ALSA_overview

Regards

Michal

Hmmm,

the test and the result

 

root@mp1-sagittarius:~# speaker-test -D hw:0,0                                  
                                                                                
speaker-test 1.2.6                                                              
                                                                                
Playback device is hw:0,0                                                       
Stream parameters are 48000Hz, S16_LE, 1 channels                               
Using 16 octaves of pink noise                                                  
Rate set to 48000Hz (requested 48000Hz)                                         
Buffer size range from 1024 to 16384                                            
Period size range from 512 to 2048                                              
Using max buffer size 16384                                                     
Periods = 4                                                                     
was set period_size = 2048                                                      
was set buffer_size = 16384                                                     
 0 - Front Left                                                                                                              
Write error: -5,Input/output error                                              
xrun_recovery failed: -5,Input/output error                                     
Transfer failed: Input/output error   

 

additionally, nothing happens on any transmission lines.

I think there is still something to do with the codec driver as Erwan suggest in the patch

"Please not that you have to get inspired by cs42l51 codecs driver to complete it"

BR Michal