cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP1 Timer

NPal.2
Senior

Hi all,

I was wondering whether we can achieve a PWM frequence of 1-3Hz with the existing timer which we have. I am targeting to generate a PWM signal within the same frequency range but using A7 as primary.

How can we achieve that ??

I do have some idea looking at the blog here : https://wiki.st.com/stm32mpu/wiki/PWM_overview

What shall be the reference period value here? How can we perform calculation for any period value?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PatrickF
ST Employee

Hi @NPal.2​ 

Did you experiment using https://wiki.st.com/stm32mpu/wiki/PWM_overview#How_to_use_PWM_with_sysfs_interface ?

1/Frequency is the Period (converted in ns) to be provided. e.g. pwm0/period (sysfs interface)

Duty_cycle is the output pulse active duration (in ns) within the Period time. e.g. pwm0/duty_cycle (sysfs interface)

I'm not expert, but I guess values in ns is limited by Linux to 32-bits, so probably 4 second period max (around 0.25Hz min).

Linux driver will compute TIM prescaler/divider/compare values according to clock provided to the timer and requested period/duty_cycle, so some rounding are present (especially on 16-bits timers).

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.