2025-05-16 2:56 AM
Hi everyone,
Hi everyone,
I’m currently designing a custom board based on the STM32MP157FAC1 evaluation board, and as part of the process, I’m working to estimate the power budget for the design.
However, I’m finding it difficult to locate clear information on load current requirements in the STM32MP1 datasheet, likely due to the MPU’s complex architecture.
Does ST provide any power estimation tools or official guidelines to help calculate power consumption when transitioning from the evaluation board to a custom design?
Any advice or references would be greatly appreciated. Thanks in advance!
2025-05-16 4:37 AM - edited 2025-05-16 4:38 AM
Hi @Rayan
Following documents are provided to help power design of your application
| AN5256 | STM32MP151, STM32MP153 and STM32MP157 discrete power supply hardware integration | AN5256.pdf |
| AN5260 | STM32MP151/153/157 MPU lines and STPMIC1B integration on a battery powered application | AN5260.pdf |
| AN5284 | STM32MP1 series system power consumption | AN5284.pdf |
Olivier
2025-05-19 4:33 AM
Document AN5284 focuses on power consumption using the STM32MP157C with the MB1263 evaluation board. I’m currently working with the MB1272 board with STM32MP157D, and it's my first time designing a Linux-based board. I was wondering if it's possible to use Linux commands, similar to those in AN5284, to check power consumption. I’d really appreciate any guidance or suggestions