cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32CubeProgrammer for basic boot chain

WHe.1
Associate II

Can I use the STM32CubeProgrammer to download ​the uboot-spl to eMMC? How can I use write the tsv file to download the uboot-spl

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Olivier GALLIEN
ST Employee

Hi @WHe.1​ ,

Can you clarify why you want to load uboot-spl in eMMC ?

I remind that uboot-spl is today only provided to be used in CubeMX DDR Tuning Tool which can load it directly in RAM.

Some useful links :

https://wiki.st.com/stm32mpu/wiki/How_to_create_your_board_device_tree#DDR_configuration_with_STM32CubeMX_DDR_Tuning_Tool

https://wiki.st.com/stm32mpu/wiki/U-Boot_SPL:_DDR_interactive_mode

Hope it help

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
WHe.1
Associate II

Hi Olivier GALLIEN

I want to use eMMC to boot the u-Boot in the basic boot chain mode, So I hope to write uboot-spl and u-boot to eMMC by STM32CubeProgammer, But I found all the sample is boot the TF-A from the eMMC. How can I do this ?

Thanks

Hi Olivier GALLIEN

I want to use eMMC to boot the u-Boot in the basic boot chain mode, So I hope to write uboot-spl and u-boot to eMMC by STM32CubeProgammer, But I found all the sample is boot the TF-A from the eMMC. How can I do this ?

Thanks