cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MPU ecosystem release V4.1.0 is online !

Kevin HUBER
ST Employee

STM32MPU ecosystem release V4.1.0 is online !

Dear STM32 MPU Community,

 

We are please to announce that New MP1 Ecosystem V4.1.0 is available.

It contains :

  • openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23 - Updated
    • STM32CubeMP1-v1.6.0
    • STM32CubeIDE-v1.11.0 - Updated
    • STM32CubeMX-v6.7.0 - Updated
    • STM32CubeProgrammer v2.12.0 - Updated
    • STM32PROGFW-UTIL-v1.0.2 - Updated

Please check out the STM32_MPU_ecosystem_release_note_-_v4.1.0 on STM32 Wiki to get complete description of content and new features.

*** Main NEW features of the STM32MP1-ecosystem-v4.1.0 release ***

  • Kernel drivers Real Time ready
  • SPI Slave support in Linux®
  • ADC oversampling support on Linux®
  • SPI master driver with dual-qspi mode in Linux® kernel support
  • DMA support for CRYP IP (Crypto performance improvement)
  • Firmware update on NAND devices
  • Improve FIP management on NAND devices
  • Add GPIO regulators driver in TF-A
  • Use FCONF to manage the Chain of Trust
  • ADC driver implementation
  • IRQ forwarding
  • HUK implementation
  • Update regulator IO management

Of course, the Wiki for previous ecosystems are still available :

 

Hope you will enjoy this new release.

In case any questions, issues .. this Community is made for you !

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NEW ! Sidekick STM32 AI agent, see here
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0