2021-06-16 3:18 AM
We would like to implement a dual partitioning system and I am trying to find out if it is possible to have a secondary SSBL (u-boot) partition in trusted mode (eMMC).
I don't see any problems for bootfs, vendorfs, rootfs and userfs. FSBL is already redundant, but I could not find anything about having a secondary SSBL partition. Is that possible? Also, if it is possible to have a secondary SSBL partition, how can I tell FSBL to use a determined SSBL partition? From what I could see in the TF-A code, that is not possible, just want a confirmation.
For context, all this is for updating a set of partitions when updating a device and switch to this set of partitions in the next boot.
Thanks.
2021-06-21 2:47 AM
Hi @Community member ,
It is possible, but you will have to implement the mechanism to select the SSBL inside the FSBL.
I suppose you can use EXT_CSD from eMMC to select the FSBL, and the bootcount can be managed through a Backup registers (see TAMP_BKP21R).
BR,
Christophe