2024-04-08 2:51 PM
I am getting a buffer ID parsing error every once in a while in the rpmsg_sdb_decode_rxbuf_string() function. It looks like the strsep fails to parse out the ID. This also is only happening on buffer ID 0. Here is the debug from the function.
What would cause strsep to truncate the string? Even when the passed in string is correct.
Before and after the error. Thanks for any help.
Apr 8 20:35:08.378 kernel(debug): rpmsg_sdb(rpmsg_sdb_decode_rxbuf_string): rxbuf_str:B00L00002000
Apr 8 20:35:08.378 kernel(debug): rpmsg_sdb(rpmsg_sdb_decode_rxbuf_string): sub_str:B00
Apr 8 20:35:08.478 kernel(debug): [265795.660533] rpmsg_sdb(rpmsg_sdb_decode_rxbuf_string): rxbuf_str:B00L00002000
Apr 8 20:35:08.478 kernel(debug): [265795.660553] rpmsg_sdb(rpmsg_sdb_decode_rxbuf_string): sub_str:B
Apr 8 20:35:08.588 kernel(err): [265795.660569] rpmsg_sdb(ERROR): Extract of buffer id failed(-22)
Apr 8 20:35:08.588 kernel(debug): [265795.760504] rpmsg_sdb(rpmsg_sdb_decode_rxbuf_string): rxbuf_str:B00L00002000
Apr 8 20:35:08.588 kernel(debug): [265795.765075] rpmsg_sdb(rpmsg_sdb_decode_rxbuf_string): sub_str:B00
2024-04-26 12:56 AM
Hi @GHamm.2 ,
The problem that you described looks like the one that was corrected in the commit "Rectify parameters passed to strsep to avoid error EINVAL (#6)" (SHA1 17c7cc20f3fc8aad8af5acafd3d0b4472004d22d) of the https://github.com/STMicroelectronics/meta-st-stm32mpu-app-logicanalyser.git Git repository.
If you uses a version of meta-st-stm32mpu-app-logicanalyser that doesn't include this commit, it might be interesting to integrate this patch or to use a more recent version.
Hope it helps.
Regards,
JC.
2024-11-27 4:18 AM
Hi, buddy, I have the same problem as you. Have you found a final solution?