2021-11-24 1:33 AM
I found the following errors when I burned kernel alone and starterpackage. May I ask why this was caused? The kernel is through https://github.com/STMicroelectronics/meta-st-stm32mp/blob/dunfell/recipes-kernel/linux/linux-stm32mp/README.HO W_to.txt teaching burn, Starterpackage is delivered via STM32_Programmer_CLI -c port= USb1 -w Flashlayout_st - image - weston/trusted/FlashLayout_sdcard_stm32mp157c - dk2 - trusted. TSV
2021-11-25 1:25 AM
I find that sometimes it can be successfully burned and sometimes it is not successful. I don't know if it is the board problem. I don't know if you want to
2021-11-25 2:14 AM
Hi @Ffu.1 ,
What is your SDcard reference also ? Can you try another one ?
Seems you flash from Linux station ? Which OS ?
Thanks
Olivier