cancel
Showing results for 
Search instead for 
Did you mean: 

Procedure to Modify Schematic and Reconfigure Linux Kernel Image for STM32MP135

DEENADHAYALAN
Associate II

Dear ST Community,

I am currently modifying an existing schematic to meet my specific requirements for the STM32MP135 Linux board. In line with these hardware changes, I would like to reconfigure and modify the Linux kernel image file accordingly. I need guidance on how to adjust the pin configurations and generate a new kernel image file.

Could you please provide a step-by-step procedure for the following:

  1. Schematic Modifications:

    • How to align the software configuration with hardware changes made to the schematic (e.g., GPIO, peripherals, or pin functions).
  2. Reconfiguration of Pin Settings in Kernel:

    • How to locate and modify the required device tree files or pin control configurations to reflect changes in the schematic.
    • Steps to adjust GPIO pin settings and peripherals in the kernel.
  3. Kernel Compilation:

    • Commands or toolchains required to recompile the kernel after modifications.
    • Guidance on rebuilding the Device Tree Blob (DTB) and compiling the kernel image.
  4. Deploying the New Kernel Image:

    • How to flash the newly compiled kernel image onto the STM32MP135 board.

Your insights and any related documentation links would be greatly appreciated.

Best regards,
DEENADHAYALAN E,
R&D Executive Engineer at EM-TECH.

WhatsApp Image 2024-09-25 at 10.30.31_607e211b.jpg

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Olivier GALLIEN
ST Employee

Hi @DEENADHAYALAN 

 

Here is some pointers : 

Wiki stm32mpu

Knowledge Article in Community : STM32 MPUs - STMicroelectronics Community

 

Hope it help 

 

Olivier 

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @DEENADHAYALAN 

 

Here is some pointers : 

Wiki stm32mpu

Knowledge Article in Community : STM32 MPUs - STMicroelectronics Community

 

Hope it help 

 

Olivier 

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.