cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple camera interfacing

KLe T.1
Associate

Hi all,

I understand that it is possible to interface a CSI2 camera sensor with the camera interface of STM32MP1 using STMIPID02 chipset. Even-though this later support 2 cameras, I'd like to know that it is feasible from the MPU's point of view ?

Thanks in advance,

Khang

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
OlivierK
ST Employee

​Hello,

Even though the STMIPID02 can supports 2 physical camera sensors, it does not support interleaving, and the STM32MP1 DCMI has only one parallel port.  It is possible to switch from one sensor to the other but it won't be on-the-fly, the DT and driver will need to be modified too.

Best Regards,

Olivier

KLe T.1
Associate

Hi Olivier,

Thank you very much for your confirmation.

Best,

Khang