MicroSD initialization timeout. When inserting the sd card, dmseg shows
"mmc0: error -110 whilst initialising SD card" With some logs, i see that mmc_send_app_op_cond is the function that timeouts.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-10-27 8:59 AM
My device tree is the following:
&sdmmc1 {
pinctrl-names = "default", "opendrain", "sleep";
pinctrl-0 = <&sdmmc1_b4_pins_a>;
pinctrl-1 = <&sdmmc1_b4_od_pins_a>;
pinctrl-2 = <&sdmmc1_b4_sleep_pins_a>;
cd-gpios = <&gpiog 1 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
disable-wp;
cd-debounce-delay-ms = <500>;
no-1-8-v;
max-frequency = <1000000>;
//st,sig-dir;
//st,neg-edge;
//st,use-ckin;
bus-width = <4>;
vmmc-supply = <&vdd_sd>;
//vqmmc-supply = <&sd_switch>;
sd-uhs-sdr12;
sd-uhs-sdr25;
sd-uhs-sdr50;
sd-uhs-ddr50;
status = "okay";
};
Sd schematics is the following:
- Labels:
-
STM32MP15 Lines
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-10-29 12:13 AM
Hi,
I copy below the STM32MP157F-DK2 Device tree portion which could help.
&sdmmc1 {
pinctrl-names = "default", "opendrain", "sleep";
pinctrl-0 = <&sdmmc1_b4_pins_a>;
pinctrl-1 = <&sdmmc1_b4_od_pins_a>;
pinctrl-2 = <&sdmmc1_b4_sleep_pins_a>;
cd-gpios = <&gpiob 7 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
disable-wp;
st,neg-edge;
bus-width = <4>;
vmmc-supply = <&v3v3>;
status = "okay";
};
please remove all the sd-uhs-***; which refer to 1.8V signalling not supported with your HW.
please add st,neg-edge;
not sure max-frequency = ; is needed. please refer also to this article in case of issue about SDMMC frequencies: https://community.st.com/s/article/FAQ-STM32MP1-how-to-setup-the-SDMMC-CK-clock-frequency-in-Linux
Regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-10-29 2:10 AM
Hi @PatrickF​
removing the st,* and all the sd-uhs* properties was not enough, I had to add
/delete-property/ st,sig-dir;
/delete-property/ st,use-ckin;
/delete-property/ sd-uhs-sdr12;
/delete-property/ sd-uhs-sdr25;
/delete-property/ sd-uhs-sdr50;
/delete-property/ sd-uhs-ddr50;
now I can see the SD.
At times, i see still the error after removing the card:
[ 64.185572] mmc0: new high speed SDHC card at address e624
[ 64.199567] mmcblk0: mmc0:e624 SS16G 14.8 GiB
[ 64.209597] mmcblk0: p1
[ 65.218871] mmc0: card e624 removed
[ 65.338268] mmc0: error -110 whilst initialising SD card
thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-10-29 2:20 AM
Maybe this is resolved by adding cd-debounce-delay-ms = <>;
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-10-29 6:42 AM
Yes, sound a logical solution. We have not that 'debounce' on our boards because the SD-Card is the boot source and not expected to be removed.
Btw, I'm puzzle regarding your need to use the "/delete-property/" on your DT as those tags are not present by default in the DT.
Maybe double check that you are not including/using some other (then unwanted) Device Tree (from e.g. EV1 board which has a level shifter on SD-Card).
The wrong import of other boards DT might create issues on other peripherals.
Regards.