2021-09-18 2:46 AM
I'm build an image for Azure IOT on STM32MP157C-DK2, following this tutorial: https://wiki.st.com/stm32mpu/wiki/How_to_integrate_Azure_IoT_Edge_on_OpenSTLinux
but I have follow error:
| error: attributes are not yet allowed on `if` expressions
| --> /usr/src/debug/iotedge-daemon/1.1.6-r0/iotedge-1.1.6/vendor/sysinfo/src/utils.rs:27:5
| |
| 27 | #[allow(clippy::identity_conversion)]
| | ^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
|
| error: aborting due to previous error
|
| error: could not compile `sysinfo`.
There is a possible solution?
Looking a similar issues, it seem a problem of version of Rust: https://github.com/Frederick888/git-credential-keepassxc/issues/12
There is a way to udate the Rust version used for build?
2021-09-23 1:35 PM
Thank you.
I successfully build with latest version of iotedge with follow commits:
meta-virtualization = dunfell 9e9868ef3d6e5da7f0ecd0680fcd69324593842 (latest)
meta-iotedge = 6840cf2afb51b4f2c535a05d5635736652f664f7 (latest)
meta-rust = 4b151fa804b1e78af445037e4136c133ada40a0 (rust == 1.47)
Just a one more question:
I changed ROOTFS_PARTITION_SIZE in /layers/meta-st/meta-st-stm32mp/conf/machine/include/st-machine-common-stm32mp.inc in order to increase the size of system partition (i.e. 8 gb), but once created the flash that change has not effect (the root partition is always 1.9 gb):
Filesystem Size Used Avail Use% Mounted on
devtmpfs 147M 0 147M 0% /dev
/dev/mmcblk0p6 1.9G 1.6G 222M 88% /
tmpfs 214M 64K 214M 1% /dev/shm
tmpfs 214M 8.8M 205M 5% /run
tmpfs 214M 0 214M 0% /sys/fs/cgroup
tmpfs 214M 52K 214M 1% /tmp
/dev/mmcblk0p4 58M 14M 40M 27% /boot
tmpfs 214M 192K 214M 1% /var/volatile
/dev/mmcblk0p5 15M 6.8M 6.7M 51% /vendor
/dev/mmcblk0p7 13G 1.6G 11G 14% /usr/local
tmpfs 43M 0 43M 0% /run/user/0
how can I change the size of root partition?
2021-09-23 10:34 PM
Hello @EBelt.1
Once again a good piece of news!
About your questions related to the increase of the ROOTFS_PARTITION_SIZE, do you also update IMAGE_ROOTFS_MAXSIZE in the same file so its value is bigger or equal to ROOTFS_PARTITION_SIZE?
Hope it helps.
Best regards,
--JM