2022-10-17 11:12 PM
In AN5031 Rev4,
Figure 49. Gigabit Ethernet 2-port switch example with VDD = 3.3 V (RTL8363NB-VG)
There is the RTL8363NB used, but I can't find the driver anywhere.
Can you provide the driver file or tell me where it is?
2022-10-27 9:23 AM
Hi @ykim.3 ,
Driver supposed to be provided by Realtek .. and most of the time up-streamed in Linux kernel.
I would be surprise it was not already supported by our latest OpenSTlinux based on kernel 5.15 ?
Did you try a "menuconfig" then search for realtek or RGMII drivers ?
Hope it help
Olivier