cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157 Custom Board Boot Failure: ERROR: DDR addr bus test & PANIC at BL2

mittyan321
Associate II

Hello,

I have developed a custom board using the STM32MP157DAA1. When I try to write the boot image, the process stops after writing fsbl-boot and does not proceed to the next step.

I checked the output from the debug port and received the following log:

NOTICE:  CPU: STM32MP157DAA Rev.Z
NOTICE:  Model: STMicroelectronics custom STM32CubeMX    board - openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11
INFO:    PMIC version = 0x21
INFO:    Reset reason (0x15):
INFO:      Power-on Reset (rst_por)
INFO:    FCONF: Reading TB_FW firmware configuration f    file from: 0x2ffe2000
INFO:    FCONF: Reading firmware configuration informa   tion for: stm32mp_fuse
INFO:    FCONF: Reading firmware configuration informa   tion for: stm32mp_io
INFO:    Using USB
INFO:      Instance 2
INFO:    Boot used partition fsbl1
NOTICE:  BL2: v2.10-stm32mp1-r2.0(debug):()
NOTICE:  BL2: Built : 11:48:32, Oct 29 2025
INFO:    BL2: Doing platform setup
INFO:    RAM: DDR3-DDR3L 16bits 533000kHz
ERROR:   DDR addr bus test: can't access memorPANIC at    PC : 0x2ffed13d

Exception mode=0x00000016 at: 0x2ffed13d

As shown in the log, a PANIC occurs immediately after the ERROR: DDR addr bus test: can't access memor.

I am currently reviewing the TF-A device tree configuration, but I haven't been able to identify the cause. Does this error indicate that the DDR memory is not working correctly?

I am using the same DDR memory part number as the evaluation board: MT41K256M16TW-107_IT_P_TR.

Could you please provide any advice on what I should check or what the potential cause might be?

Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions

Hello sabry,

Thank you for your message.

I managed to resolve the issue on my end. The problem was an error where the PMIC's PWRCTRL signal was not being set HIGH. After correcting this hardware issue, I used the STM32DDRFW-UTIL tool to tune the DDR, and it is now working successfully.

I apologize for the confusion, as my problem was ultimately not related to the Device Tree configuration I originally suspected. Thank you for reaching out.

Regards

View solution in original post

2 REPLIES 2
sabry
Associate

Hello mittyan321,

I’m currently working on a custom board based on the MYC-YA15XC-T (STM32MP151A) module, and I’m facing a similar situation during bring-up.

I saw that in your case, you had the DDR initialization issue (ERROR: DDR addr bus test: can't access memory) and mentioned you were checking the TF-A Device Tree configuration.

Could you please share how you configured the Device Tree (TF-A and U-Boot parts) for your custom board?
Specifically:

Did you start from the CubeMX generated .dts or from the EV1 / DK2 reference?

Which files did you modify to match your DDR configuration (e.g. stm32mp15-ddr.dtsi, tf-a device-tree)?

Did you have to adjust any parameters under the &rcc or &ddr nodes to make it work?

It would be really helpful to see an example of your setup, since I’m trying to validate my own device tree for a board using a similar memory part and PMIC (STPMIC1).

Thank you in advance for your feedback

sabry

Hello sabry,

Thank you for your message.

I managed to resolve the issue on my end. The problem was an error where the PMIC's PWRCTRL signal was not being set HIGH. After correcting this hardware issue, I used the STM32DDRFW-UTIL tool to tune the DDR, and it is now working successfully.

I apologize for the confusion, as my problem was ultimately not related to the Device Tree configuration I originally suspected. Thank you for reaching out.

Regards