2023-05-26 5:55 AM
Hi, I use boot1 pin as gpio key function. The boot1 is PI5, and I configure it in kernel dts code. When the system boot up, the input event0 device is shows, but I use hexdump can not get any key code data. Currently, my board is boot from sdcard.
gpio-keys {
compatible = "gpio-keys";
#size-cells = <0>;
user {
label = "user";
linux,code = <BTN_1>;
gpios = <&gpioi 5 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
};
};
2023-05-29 7:57 AM
Hello @Community member ,
Are you on a custom board or a board provided by ST?
Best Regards,
Kevin
2023-06-01 8:19 AM
My custom board. I try to use boot mode pin as gpio to input/output.