2021-04-09 07:52 AM
I used the latest official version(2021-03-31) to configure the stm32mp157c-dk2 of the optee version, and used the official tutorial to generate fip.bin and burn it to the corresponding partition, but it seems that the image is not checked,in other worlds, I did not see the successful prompt for the verification of the mirror image.
Solved! Go to Solution.
2021-04-19 01:08 AM
Hi @DDing.1 ,
Go to know, in the FIP management there is no formal "Authentication success" to be printed.
If it boots, it works ;)
The only way can you can ensure that it works is that the complete firmware + certificate are loaded:
Image 31 (FW_CONFIG) required Image 6 (Trusted Boot Firmware Certificate).
You have mode loaded images (ID must correspond to all certificates) to confirm that it works.
There is no possibility to skip the authentication so if OP-TEE/U-Boot are launched, authentication is successful.
BR,
Lionel
2021-04-09 08:19 AM
Hi @DDing.1 ,
I understand you expect FIP binaries to be authenticate, right ?
Please refer to https://wiki.st.com/stm32mpu/wiki/How_to_configure_TF-A_FIP#Secure_boot
Hope it help
Olivier
2021-04-09 08:27 AM
Yes, I configured it according to this (use the TF-A makefile), but I did not see the corresponding verification process when stm32 was started(the startup log did not seem to change). I want to know if I I have forgotten any steps,thanks
2021-04-10 05:30 AM
Hi @DDing.1 ,
According to your traces, the FIP seems to be properly generated BUT the BL2 is not build with the TRUSTED_BOARD_BOOT=1 support. So the processing to load associated certificate chain is not supported in your current BL2 TF-A binary -> No authentication.
To ensure that it is properly on, there is a trace during boot to now if the crypto_lib is initialized:
NOTICE: BL2: v2.4-r1.0(debug):v2.4-stm32mp-r1
NOTICE: BL2: Built : 12:14:26, Apr 10 2021
INFO: Using crypto library 'stm32_crypto_lib'
Please rebuild the TF-A BL2 as explained https://wiki.st.com/stm32mpu/wiki/TF-A_BL2_overview#Trusted_boot_support and reflash it.
Use:
https://wiki.st.com/stm32mpu/wiki/How_to_configure_TF-A_BL2#Build_process
Important is the
TRUSTED_BOARD_BOOT = 1: adds MBEDTLS build sources and authentication framework enabled
BR,
Lionel
2021-04-12 06:27 PM
Hello, I have now modified the configuration of BL2 according to the document and the configuration command is as follows:
make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 DTB_FILE_NAME=stm32mp157c-dk2.dtb STM32MP_SDMMC=1 STM32MP_EMMC=1 AARCH32_SP=optee TRUSTED_BOARD_BOOT=1 GENERATE_COT=1 DYN_DISABLE_AUTH=1 MBEDTLS_DIR=/home/tflgr/mbedtls
Then I configured the fip binary file again, the command is as follows:
make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 AARCH32_SP=optee
DTB_FILE_NAME=stm32mp157c-dk2.dtb
BL33=../../FIP_artifacts/u-boot/u-boot-nodtb-stm32mp15.bin
BL33_CFG=../../FIP_artifacts/u-boot/u-boot-stm32mp157c-dk2-trusted.dtb
BL32=../../FIP_artifacts/optee/tee-header_v2-stm32mp157c-dk2.bin BL32_EXTRA1=../../FIP_artifacts/optee/tee-pager_v2-stm32mp157c-dk2.bin
BL32_EXTRA2=../../FIP_artifacts/optee/tee-pageable_v2-stm32mp157c-dk2.bin
FW_CONFIG=../../FIP_artifacts/arm-trusted-firmware/fwconfig/stm32mp157c-dk2-fw-config-optee.dtb
MBEDTLS_DIR=/home/tflgr/mbedtls TRUSTED_BOARD_BOOT=1 GENERATE_COT=1
ROT_KEY=./plat/arm/board/common/rotpk/arm_rotprivk_rsa.pem fip
The following files were generated, and then put .stm32 and fip.bin into the sdb1 and sdb3 partitions with the dd command.
But the startup log did not change and did not output INFO: Using crypto library 'stm32_crypto_lib', as follows:
NOTICE: CPU: STM32MP157CAC Rev.B
NOTICE: Model: STMicroelectronics STM32MP157C-DK2 Discovery Board
NOTICE: Board: MB1272 Var2.0 Rev.C-01
INFO: Reset reason (0x14):
INFO: Pad Reset from NRST
INFO: PMIC version = 0x10
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe3000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.4-r1.0(debug):v2.4-dirty
NOTICE: BL2: Built : 16:43:51, Nov 17 2020
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
WARNING: Couldn't find property st,phy-cal in dtb
INFO: Memory size = 0x20000000 (512 MB)
INFO: BL2: Loading image id 31
INFO: Loading image id=31 at address 0x2ffff000
INFO: Image id=31 loaded: 0x2ffff000 - 0x2ffff1fa
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewal
WARNING: FCONF: Invalid config id 26
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffc0000
INFO: Image id=4 loaded: 0x2ffc0000 - 0x2ffc002c
INFO: OPTEE ep=0x2ffc0000
INFO: OPTEE header info:
Thanks.
2021-04-12 11:02 PM
Hi,
Your build command looks go to me, but I'm surprised that the build date print into your boot is NOTICE: BL2: Built : 16:43:51, Nov 17 2020.
Are you sure to updated it into your card? First partition must be updated with you binary generated, stm32 file.
I'm surprised as, regarding your build command, you will generate a release version (without all these logs)?
Could you please confirm.
DYN_DISABLE_AUTH=1 -> Not mandatory, you could remove it from now or maybe double check that the property is still set to 0 in the DT file to avoid any removal of the authentication.
GENERATE_COT=1 -> Used to generate the FIP, not required during the BL2 build.
BR,
Lionel
2021-04-14 04:58 AM
Thanks, I found a problem with the Ubuntu system last time that dd was not copied into the mirror. This time after successfully copied into the image, the following error occurred:
NOTICE: CPU: STM32MP157CAC Rev.B
NOTICE: Model: STMicroelectronics STM32MP157C-DK2 Discovery Board
NOTICE: Board: MB1272 Var2.0 Rev.C-01
INFO: Reset reason (0x14):
INFO: TF-A simple example
INFO: TF-A simple example
INFO: Pad Reset from NRST
INFO: PMIC version = 0x10
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffdd000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: FCONF: Reading firmware configuration information for: tbbr
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.4-r1.0(debug):
NOTICE: BL2: Built : 02:33:15, Apr 14 2021
INFO: Using crypto library 'stm32_crypto_lib'
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
WARNING: Couldn't find property st,phy-cal in dtb
INFO: Memory size = 0x20000000 (512 MB)
INFO: BL2: Loading image id 31
INFO: Loading image id=6 at address 0x2ffff000
INFO: Image id=6 loaded: 0x2ffff000 - 0x2ffff4b6
ERROR: BL2: Failed to load image id 31 (-80)
After adjusting the log input level to 50, the following problems occur:
INFO: BL2: Loading image id 31
VERBOSE: FIP header looks OK.
INFO: Loading image id=6 at address 0x2ffff000
INFO: Image id=6 loaded: 0x2ffff000 - 0x2ffff4b6
VERBOSE: BSEC: OTP 0 is locked and will not be refreshed
VERBOSE: crypto_verify_signature: mbedtls_oid_get_sig_alg (-46)
ERROR: BL2: Failed to load image id 31 (-80)
I found something about mbedtls in the tf-a package, but it doesn’t seem to be available, so I use mbedtls from https://github.com/ARMmbed/mbedtls.git. Could this be the reason for the startup failure?
2021-04-14 11:59 AM
Hi @[DDing.1] ,
The wiki as a lack of info, I'll add it soon for the MBEDTLS part.
MBEDTLS is used as an external repo as mentioned here in the official doc:
https://trustedfirmware-a.readthedocs.io/en/v2.4/design/trusted-board-boot-build.html
To build the FIP image, ensure the following command line variables are set while invoking
make to build TF-A:
MBEDTLS_DIR=<path of the directory containing mbed TLS sources>
TRUSTED_BOARD_BOOT=1
GENERATE_COT=1
As per requirement:
https://trustedfirmware-a.readthedocs.io/en/v2.4/getting_started/prerequisites.html
The following libraries are required for Trusted Board Boot support:
mbed TLS == 2.24.0 (tag: mbedtls-2.24.0)
So now, regarding your issue (because it seems that your build is now OK as the crypto lib is initialized).
It seems internal MBEDTLS error. Could you please double check the version used to build your BL2 and confirm that it's the 2.24.0?
BR,
Lionel
2021-04-14 08:02 PM
Thanks.But I rebuilt the image with version 2.24.0, but it still got the same error.
2021-04-15 07:20 AM
I found that the size of bl2.bin compiled from fip.bin is different from the size of bl2.bin produced by compiling bl2. If fip image is generated firstly and then compile bl2.bin , the following error will occur:
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffdd000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
VERBOSE: FCONF: stm32mp-io_policies.fw_cfg_uuid found with value = 0x6ae10758 0d
VERBOSE: FCONF: stm32mp-io_policies.bl32_uuid found with value = 0x89e1d005 0x4b
VERBOSE: FCONF: stm32mp-io_policies.bl32_extra1_uuid found with value = 0x9bc272
VERBOSE: FCONF: stm32mp-io_policies.bl32_extra2_uuid found with value = 0xb17ba5
VERBOSE: FCONF: stm32mp-io_policies.bl33_uuid found with value = 0xa7eed0d6 0x42
VERBOSE: FCONF: stm32mp-io_policies.hw_cfg_uuid found with value = 0xd9f1b808 0b
VERBOSE: FCONF: stm32mp-io_policies.tos_fw_cfg_uuid found with value = 0x1a7c250
VERBOSE: FCONF: stm32mp-io_policies.nt_fw_cfg_uuid found with value = 0x1598da20
WARNING: Couldn't find property t_boot_fw_cert_uuid in dtb
WARNING: FCONF: Read cell failed for t_boot_fw_cert_uuid
PANIC at PC : 0x2ffe4dad
If first generate bl2 and then generate fip, the previous error will occur. Is there a problem when generating bl2.bin, or is the link dtb and bin incorrect?