cancel
Showing results for 
Search instead for 
Did you mean: 

Has anyone faced issue about bluetooth connectivity on stm32mp157c, error details in description below:

rahuj.1
Associate II

ERROR:dbus.connection:Exception in handler for D-Bus signal:

Traceback (most recent call last):

 File "/usr/lib/python3.8/site-packages/dbus/connection.py", line 232, in maybe_handle_message

  self._handler(*args, **kwargs)

 File "/home/root/0.3.4.5/obd_gen2_ble_py/blemodule/adapter.py", line 285, in _properties_changed

  self.address == adapter_addr,

 File "/home/root/0.3.4.5/obd_gen2_ble_py/blemodule/adapter.py", line 104, in address

  return self.adapter_props.Get(constants.ADAPTER_INTERFACE, 'Address')

 File "/usr/lib/python3.8/site-packages/dbus/proxies.py", line 141, in __call__

  return self._connection.call_blocking(self._named_service,

 File "/usr/lib/python3.8/site-packages/dbus/connection.py", line 652, in call_blocking

  reply_message = self.send_message_with_reply_and_block(

dbus.exceptions.DBusException: org.freedesktop.DBus.Error.NoReply: Message recipient disconnected from message bus without replying

ERROR:dbus.connection:Exception in handler for D-Bus signal:

Traceback (most recent call last):

 File "/usr/lib/python3.8/site-packages/dbus/bus.py", line 177, in activate_name_owner

  return self.get_name_owner(bus_name)

 File "/usr/lib/python3.8/site-packages/dbus/bus.py", line 361, in get_name_owner

  return self.call_blocking(BUS_DAEMON_NAME, BUS_DAEMON_PATH,

 File "/usr/lib/python3.8/site-packages/dbus/connection.py", line 652, in call_blocking

  reply_message = self.send_message_with_reply_and_block(

dbus.exceptions.DBusException: org.freedesktop.DBus.Error.NameHasNoOwner: Could not get owner of name 'org.bluez': no such name

During handling of the above exception, another exception occurred:

Traceback (most recent call last):

 File "/usr/lib/python3.8/site-packages/dbus/connection.py", line 232, in maybe_handle_message

  self._handler(*args, **kwargs)

 File "/home/root/0.3.4.5/obd_gen2_ble_py/blemodule/adapter.py", line 281, in _properties_changed

  adapter_addr = dbus_tools.get_adapter_address_from_dbus_path(path)

 File "/home/root/0.3.4.5/obd_gen2_ble_py/blemodule/dbus_tools.py", line 119, in get_adapter_address_from_dbus_path

  mngd_objs = get_managed_objects()

 File "/home/root/0.3.4.5/obd_gen2_ble_py/blemodule/dbus_tools.py", line 88, in get_managed_objects

  manager = dbus.Interface(bus.get_object(constants.BLUEZ_SERVICE_NAME, '/'),

 File "/usr/lib/python3.8/site-packages/dbus/bus.py", line 241, in get_object

  return self.ProxyObjectClass(self, bus_name, object_path,

 File "/usr/lib/python3.8/site-packages/dbus/proxies.py", line 250, in __init__

  self._named_service = conn.activate_name_owner(bus_name)

 File "/usr/lib/python3.8/site-packages/dbus/bus.py", line 182, in activate_name_owner

  self.start_service_by_name(bus_name)

 File "/usr/lib/python3.8/site-packages/dbus/bus.py", line 277, in start_service_by_name

  return (True, self.call_blocking(BUS_DAEMON_NAME, BUS_DAEMON_PATH,

 File "/usr/lib/python3.8/site-packages/dbus/connection.py", line 652, in call_blocking

  reply_message = self.send_message_with_reply_and_block(

dbus.exceptions.DBusException: org.freedesktop.systemd1.ShuttingDown: Refusing activation, D-Bus is shutting down.

Release

2022-11-28 16:42:12,298 - blemodule.adapter - ERROR - No Bluetooth Adapater Found

Traceback (most recent call last):

 File "/home/root/0.3.4.5/obd_gen2_ble_py/main.py", line 5, in <module>

  from Mqttmodule.mqtt import *

 File "/home/root/0.3.4.5/obd_gen2_ble_py/Mqttmodule/mqtt.py", line 6, in <module>

  from eventHandler.handler import *

 File "/home/root/0.3.4.5/obd_gen2_ble_py/eventHandler/handler.py", line 5, in <module>

  from blemodule.ble import *

 File "/home/root/0.3.4.5/obd_gen2_ble_py/blemodule/ble.py", line 8, in <module>

  from blemodule import adapter, peripheral, constants, dbus_tools, device, tools

 File "/home/root/0.3.4.5/obd_gen2_ble_py/blemodule/peripheral.py", line 15, in <module>

  bus = dbus.SystemBus()

 File "/usr/lib/python3.8/site-packages/dbus/_dbus.py", line 195, in __new__

  return Bus.__new__(cls, Bus.TYPE_SYSTEM, mainloop=mainloop,

 File "/usr/lib/python3.8/site-packages/dbus/_dbus.py", line 102, in __new__

  bus = BusConnection.__new__(subclass, bus_type, mainloop=mainloop)

 File "/usr/lib/python3.8/site-packages/dbus/bus.py", line 124, in __new__

  bus = cls._new_for_bus(address_or_type, mainloop=mainloop)

dbus.exceptions.DBusException: org.freedesktop.DBus.Error.NoReply: Did not receive a reply. Possible causes include: the remote application did not send a reply, the message bus security policy blocked the reply, the reply timeout expired, or the network connection was broken.

0 REPLIES 0