cancel
Showing results for 
Search instead for 
Did you mean: 

Debian based linux distro on STM32MP135-DK

embeddedGeek
Associate II

I wonder if i can run debian based distro, lets say ubuntu on STM32MP135-dk. 

If yes, Is there any example project i can check?

1 ACCEPTED SOLUTION

Accepted Solutions
Olivier GALLIEN
ST Employee

Hi @embeddedGeek ,

 

Thanks for your post. 

Nothing officially supported by ST. 

I guess you can find some attempt/prototype here and there on the web for MP15. 

MP13, without GPU is probably less fitted to meet the performance requirement. 

 

In order to ST to beter capture the need, could you please elaborate further project/product you are targeting?

 

Thanks

 

Olivier 

 

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @embeddedGeek ,

 

Thanks for your post. 

Nothing officially supported by ST. 

I guess you can find some attempt/prototype here and there on the web for MP15. 

MP13, without GPU is probably less fitted to meet the performance requirement. 

 

In order to ST to beter capture the need, could you please elaborate further project/product you are targeting?

 

Thanks

 

Olivier 

 

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.