2021-06-03 12:59 AM
I'm trying to use an ADV7280 videodecoder with DCMI and embedded linux on a board based on STM32157c-dk2. The decoder should output 720x576 picture resolution with the camera (PAL,CV) attached. However the DCMI seems to be in 'normal mode' which allows max 480x272 resolution based on app. note AN5020. How to change mode to circular buffer mode which should allow higher resolutions? I haven't found any linux device tree setups for that. Some settings for dma or dcmi ? Examples?
2021-06-03 1:34 AM
Hi,
Have you looked to https://wiki.st.com/stm32mpu/wiki/DCMI_device_tree_configuration#DT_configuration_examples
and https://wiki.st.com/stm32mpu/wiki/V4L2_camera_overview ?
Camera sensor connected to DCMI is available on EV1 board with running example in starter package.
Under Linux, DCMI performance is constrained by HW and SW and effective resolution and frame-rate is limited.
Was tested ok with few resolution and frame rate, e.g. 720x480 @30fps, 1280x720 @27fps, so 720x576 should be ok @30fps.
Regards.
2021-06-03 4:32 AM
Yes the example in starter package works ok. Maybe the issue is some linux driver problem? I have used the driver adv7180 which should be ok with adv7280. If I try to change the resolution with v4l2-ctl, it doesn't change. And adv7180 sub device driver for stm32-dcmi does not announce "not using libv4l2" as the EV1 does with ov5640 driver.
2021-06-28 1:24 AM
When trying to start a capture with Gstreamer there are error messages : "dma dma0chan2: nb items not supported" and "stm32-dcmi 4c006000.dcmi: dcmi_start_dma: DMA dmaengine_prep_slave_single failed for buffer phy=0xc7c00000 size=691200" . It seems that it has something to do with memory allocation. I haven't found the reason why these drivers are acting differently (adv7180 vs. ov5640)
2021-07-01 12:46 AM
Is anyone using a camera with DCMI other than ov5640 or some videodecoder?
2021-07-02 6:00 AM
Hello Ronte.1 (Community Member),
Did you manage to change the resolution with v4l2-ctl? The FPS and resolution needs to be explicitely mentionned in the driver.
There is an app note AN5470 (still using the OV5640 but via the STMIPID02 MIPI CSI2 deserializer), it gives also some debugging tips with a new sensor.
Regarding Gtreamer issues, please refer to https://wiki.st.com/stm32mpu/wiki/Gst-play
gtksink offers slow performance since it supports only RGB 32-bit and does not provide DMA buffer pool so that extra frame copy kills performance.
Regards,
2021-08-02 1:14 AM
The driver is setting fixed resoltution 720x576 and FPS 25Hz. If I try to change the resolution with v4l2-ctl it doesn't change. If I try to capture video with gst-launch-1.0 I get errors mentioned above.
2023-12-29 12:24 PM - edited 2023-12-29 12:25 PM
Hi,
I have same issue, capture 480x272 or smaller seems find, but higher then I have same error message:
""dma dma0chan2: nb items not supported" and "stm32-dcmi 4c006000.dcmi: dcmi_start_dma: DMA dmaengine_prep_slave_single failed for buffer..."
did you find the solution for this issue?