2024-12-10 4:35 PM
On an STM32MP157D-based system, I wish to condition the Linux CLOCK_REALTIME precision clock against an external clock source in a non-standard manner (ie. not using PTPD or similar).
To do this, I am using a wireless radio controlled by the CM4 core on the STM32MP157D to synchronize and condition the 64-bit Ethernet precision timer within a microsecond of a clock on the far end of the wireless connection. This code was adapted from an STM32F767 device, and the port was relatively easy to do.
Can I configure the Linux system to use the Ethernet precision timer rather than the default system timer for the CLOCK_REALTIME precision clock? If so, how might I configure this within the kernel or device tree files?
Alternatively, how might I adjust the CM4 ARM Cortex-A Generic Timer, which is likely used by default for CLOCK_REALTIME, so that it can be set and adjusted by code running within the CM4 core? Or is some other clock used by Linux for the CLOCK_REALTIME clock?
Thanks,
Mike
2024-12-10 5:09 PM
By the way, I can read the synchronized Ethernet precision timer from a Linux application using the /dev/ptp0 device using the code below. However, it would be best for my purposes if I could get the Linux system clock to use this timer for the CLOCK_REALTIME clock.
#include <time.h>
#include <fcntl.h>
#include <stdio.h>
#include <unistd.h>
#include <linux/ptp_clock.h>
#include <sys/ioctl.h>
#define FD_TO_CLOCKID(fd) ((~(unsigned int)(fd) << 3) | 3)
int main() {
// Open the PHC device (e.g., /dev/ptp0)
int fd = open("/dev/ptp0", O_RDONLY);
if (fd < 0) {
perror("Failed to open PHC device");
return -1;
}
// Convert file descriptor to clock ID
clockid_t clk_id = FD_TO_CLOCKID(fd);
// Use clock_gettime to fetch the current time from the PHC
struct timespec ts;
if (clock_gettime(clk_id, &ts) < 0) {
perror("Failed to get PHC time");
close(fd);
return -1;
}
printf("PHC time: %lld.%09ld seconds\n", (long long)ts.tv_sec, ts.tv_nsec);
// Close the PHC device
close(fd);
return 0;
}