cancel
Showing results for 
Search instead for 
Did you mean: 

APB5 access in Engineering mode

SMang.1
Associate II

Hi,

Can I access APB5 bus in engineering mode to run I2C4 with I2C4_SCL = PZ4, I2C4_SCL = PZ5?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
PatrickF
ST Employee

Yes, in engineering mode, RCC is in non-secure mode, as well as all IPs secured by ETZPC (except secrets like ROM or some OTPs which are still protected). Except for memory map restrictions, this stand for Cortex-A7 and Cortex-M4.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Thanks @PatrickF​ .

Just to confirm, the clock for APB5 is derived from what core?

PatrickF
ST Employee

APB5 (pclk5) root clock usually come from PLL2 (AXI clock) with dedicated sub-dividers.

See product RefMan (e.g. RM0436 for STM32MP157), "Core and busses clock generation" in RCC section.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.