cancel
Showing results for 
Search instead for 
Did you mean: 

Anyone know of a chip/board design that has more than one ARM Cortex-M4 or M7, I need 4 of them to do serious signal processing, paired with a big brain like Cortex-A7 that runs linux to send the data to the cloud... ideally would be able to share flash

CLove.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @CLove.1​ ,

Please consider the STM32 Portfolio on st.com to analyze if a STM32 cluster board can be a solution.

For sure, STM32MP1 can be the Cortex-A7 that runs linux part.

Maybe worth also to consider those 2 links for signal processing on STM32

https://www.st.com/en/embedded-software/x-cube-dspdemo.html

https://www.st.com/resource/en/application_note/dm00273990-digital-signal-processing-for-stm32-microcontrollers-using-cmsis-stmicroelectronics.pdf

Hope it help

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
CLove.1
Associate

Yeah, already know about the signal processing libraries, thanks, it is the advanced SIMD stuff on Cotrex-M4 and M7 that I'm using - I just have a lot of signal processing to do requiring 4 cores. I see so many chips that have quad-core A7 for the main OS (linux) and only 1 Cortex-M4 which is odd, why not dual-core-A7 + dual-core-M4, or quad core A7 + quad-Core M4. The only one I can find with tons of low power signal processing cores is in the Qualcomm snapdragon, but that's way over kill for what I need...