2025-04-03 11:45 PM
Hello.
I am designing a circuit with stm32mp157f.
I'm looking for eMMC when choosing memory because 4Gbit slc nand flash is too expensive.
In the datasheet, I read in the data sheet that stm32 supports emmc.
The question is as follows.
Regards,
Youngjun.
Solved! Go to Solution.
2025-04-07 12:07 AM
Hi @Younjun
1st question answered in https://community.st.com/t5/stm32-mpus-products/can-i-use-any-kind-of-emmc-for-stm32mp1/td-p/790740
2nd question answer is No. QUADSPI of STM32MP1 only support Flash.
RAM is DDR connected on DDRCTRL/DDRPHY (external DDR is mandatory to use the platform as internal RAMs are very small)
Regards,
2025-04-07 12:07 AM
Hi @Younjun
1st question answered in https://community.st.com/t5/stm32-mpus-products/can-i-use-any-kind-of-emmc-for-stm32mp1/td-p/790740
2nd question answer is No. QUADSPI of STM32MP1 only support Flash.
RAM is DDR connected on DDRCTRL/DDRPHY (external DDR is mandatory to use the platform as internal RAMs are very small)
Regards,