Skip to main content
Younjun
Associate II
April 7, 2025
Solved

Can I use any kind of eMMC for stm32mp1?

Hello.

I am designing a circuit with stm32mp157f.

I'm looking for eMMC when choosing memory because 4Gbit slc nand flash is too expensive.

In the datasheet, I read in the data sheet that stm32 supports eMMC.

 

The question is as follows.

  • Is it correct that eMMC can be used even if it is not SLC(it's pSLC, MLC...) like IS21EF04GP-JCLI-TR?
    (It's my first time using mpu and memory. So it's very difficult for me to choose memory.)

 

Regards,

Youngjun.

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
April 7, 2025

Hi @Younjun 

eMMC error correction related to the flash used inside it is abstracted by the eMMC controller inside the memory.

You don't have to worry of this (eMMC management could be seen it is like an SSD).

All eMMC which are JEDEC compliant are supported.

Only very very small eMMC (we have seen this on a 1Gbits/128Mbytes eMMC) might need specific OTP  setting as listed here because their boot sector is smaller than expected FSBL size (including header).

PatrickF_0-1744008237397.png

No issue on a then 4GBytes you listed.

Btw, you mention 4Gbits SLC NAND and your are referring to a 4GBytes eMMC.

 

Regards.

 

 

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

2 replies

PatrickF
PatrickFBest answer
ST Employee
April 7, 2025

Hi @Younjun 

eMMC error correction related to the flash used inside it is abstracted by the eMMC controller inside the memory.

You don't have to worry of this (eMMC management could be seen it is like an SSD).

All eMMC which are JEDEC compliant are supported.

Only very very small eMMC (we have seen this on a 1Gbits/128Mbytes eMMC) might need specific OTP  setting as listed here because their boot sector is smaller than expected FSBL size (including header).

PatrickF_0-1744008237397.png

No issue on a then 4GBytes you listed.

Btw, you mention 4Gbits SLC NAND and your are referring to a 4GBytes eMMC.

 

Regards.

 

 

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Younjun
YounjunAuthor
Associate II
April 7, 2025

Hi @PatrickF 

Thank you for replying.

Yes, 4GByte is correct, not 4Gbyte. (I marked it wrong.)

Thanks to you, my curiosity was solved.
I'm trying to use eMMC over 4GByte.

Thanks

Regards,

Youngjun.