stm32mp157 Ethernet problem
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-02-20 1:19 AM
hello:
I made a board using the AR8035 phy chip. The system can find the phy, but it can't connect to the network.I need your help.
log:
Solved! Go to Solution.
- Labels:
-
STM32MP15 Lines
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-02-21 12:32 AM
I had a quick look, just ensure the PG5 receive a 125MHz from the PHY (need SW config inside the PHY to output this frequency, otherwise you get 25MHz by default on CLK_25M pin).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-02-20 2:45 AM
With the log you shared, we did not see any issue with the Ethernet, you end up at [12.232391] with a 'link-up' message.
Issue might be more on your Network Server set up. Seems you get an ipv6 address without ipv4, then you need to set manually an ipv4 address. Please look at your DHCP server config.
Did you made same tests using STM32MP157A-DK1 or STM32MP157C- DK2 board with default starter package ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-02-20 3:33 AM
- Thank you very much for your reply,But I've tested the same thing with normal networks
[ 11.585842] Micrel KSZ9031 Gigabit PHY stmmac-0:06: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=stmmac-0:06, irq=POLL)
[ 11.687613] dwmac4: Master AXI performs any burst length
[ 11.719501] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[ 11.731984] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 11.791796] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock
[ 11.844925] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 11.866000] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 11.901577] Bluetooth: hci0: BCM43430A1 (001.002.009) build 0264
[ 11.975836] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 12.112596] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac43430-sdio for chip BCM43430/1
[ OK ] Started Network Name Resolution.
[ 12.401230] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac43430-sdio for chip BCM43430/1
[ 12.491165] brcmfmac: brcmf_c_preinit_dcmds: Firmware: BCM43430/1 wl0: Sep 11 2018 09:22:09 version 7.45.98.65 (r707797 CY) FWID 01-b54727f
[ 16.002705] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 16.009802] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-02-20 5:24 AM
On my side, I cannot help much more, experts told me that it could be a DHCP or your own network config which make the ping not working.
There is no error visible in the log.
When doing ifconfig after boot and few seconds after RJ45 cable connection, you should have both inet and inet6 defined without manual action, e.g. :
root@stm32mp1-eval:~# ifconfig
eth0 Link encap:Ethernet HWaddr 00:80:E1:01:64:F9
inet addr:10.48.0.89 Bcast:10.48.3.255 Mask:255.255.252.0 <== here
inet6 addr: fe80::280:e1ff:fe01:64f9/64 Scope:Link <== here
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:68 errors:0 dropped:3 overruns:0 frame:0
TX packets:47 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:10311 (10.0 KiB) TX bytes:9222 (9.0 KiB)
Interrupt:60
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-02-20 5:21 PM
Thank you very much for your reply
Can you help me check the hardware design of the phy
The phy address is 6
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-02-21 12:32 AM
I had a quick look, just ensure the PG5 receive a 125MHz from the PHY (need SW config inside the PHY to output this frequency, otherwise you get 25MHz by default on CLK_25M pin).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-02-24 5:41 PM
Yes, it needs to be configured to 125M in the PHY driver, otherwise the default is 25M, thank you.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-03-06 7:25 PM
Thank you very much for your support, but I found a bug. I added the operation of configuring 125MHZ in the PHY driver, and found that the connection with the router could be normal, but the failure of initializing the dma if the network cable is not connected will result in failure. I measured the existence of 125MHZ in PG5.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-01-08 3:59 AM
AR8035 switches RX clock off without a cable or after some time passed.
How to reset gmac dma in absence of that clock?
Is there any official workaround for such a situation?