cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP15 ECO 5.0.0 BL2 stuck at loading BL32

debugging
Lead

Custom STM32MP157AAA3 board with 512MB DDR.

[Note: the NOTICE: DEBUG messages in below logs were added to the source code of TF-A]

The TF-A DT was compiled with option for SYSRAM with resulting dtb fw-config

debugging_0-1694663508331.png

OP-TEE was compiled for SYSRAM and and enabled with pager as can be seen in  the contents FIP file:

debugging_0-1694619876455.png

The reservation was made in OP-TEE DT:

debugging_1-1694619940511.png

The optee-header_v2.bin: file  generated:

debugging_4-1694621468535.png

Result:

NOTICE: Early console setup
NOTICE: CPU: STM32MP157AAA Rev.B
NOTICE: Model: STMicroelectronics custom STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mp1-v23.06.21
NOTICE: DEBUG: stm32_print_boardinfo
NOTICE: DEBUG: stm32mp_is_closed_device
NOTICE: HELLO: fixed_regulator_register
NOTICE: DEBUG: stm32mp1_arch_security_setup
NOTICE: DEBUG: print_reset_reason
INFO: Reset reason (0x14):
INFO: Pad Reset from NRST
NOTICE: DEBUG: stm32mp1_syscfg_enable_io_compensation_finish
NOTICE: DEBUG: fconf_populate
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
NOTICE: DEBUG: stm32_skip_boot_device_after_standby
NOTICE: DEBUG: stm32mp_io_setup
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.8-stm32mp1-r1.0(debug):()
NOTICE: BL2: Built : 15:24:01, Sep 11 2023
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
INFO: Memory size = 0x20000000 (512 MB)
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0x2ffff000
INFO: Image id=1 loaded: 0x2ffff000 - 0x2ffff1ea
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffc0000
INFO: Image id=4 loaded: 0x2ffc0000 - 0x2ffc002c
INFO: OPTEE ep=0x2ffc0000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x0
INFO: flags=0x0
INFO: nb_images=0x2
NOTICE: DEBUG: parse optee image #0
NOTICE: DEBUG: header->optee_image_list[num].image_id=0x0
NOTICE: DEBUG: OPTEE_PAGER_IMAGE_ID=0
NOTICE: DEBUG: OPTEE_PAGED_IMAGE_ID=1
NOTICE: DEBUG: init_load_addr=0x2ffc0000
NOTICE: DEBUG: init_size=0x26fc0
NOTICE: DEBUG: image_info->image_base=0x2ffc0000
NOTICE: DEBUG: image_info->image_max_size=0x22000
WARNING: The load address in optee header 0x2ffc0000 - 0x2ffe6fc0 is not in reserved area: 0x2ffc0000 - 0x2ffe2000.
ERROR: OPTEE header parse error.
PANIC at PC : 0x2ffed03d

The OP-TEE generated header file optee-header_v2.bin has the load address for FW_CONFIG (image ID 1) set to 0x2FFC0000,  that is the same address that OPTEE tries to load loading Image ID  #8 (extra 1) , also the boot log below. Changed the starting address in the OPTEE , conf.mk file to 0x2FFC0200 to avoid a conflict. (shown in the picture below) The optee-header_v2.bin has the size set to 0x26dc0 which is the size of BL32 Extra 1  (ID 8) this isis too large to load in SRAM and created an BL2 load error as above.

After changing the size in the OP-TEE .mk file to to 0x1000 the OPTEE build still set it to 0x26EC0 in the header.:

It seems the OPTEE build  ignored the config.mk file setting

OP-TEE conf.mk file:

CFG_TZSRAM_START ?= 0x2ffc0200
CFG_TZSRAM_SIZE ?= 0x00010000

The next attempt to load ID 8 (BL32 extra 1) was to manually changing the header file to size of 0x1000. 

The changed header as follows

debugging_2-1694620173650.png

This went through a bit more but an “out of bounds" error is raised. See the log below.

Questions:

1 Why does OPTEE use the same start address for image ID 8 (Extra 1) and for ID 1 (FWCONFIG) ? Is this correct ? If we had not changed the base address in the conf.mk to 0x2ffc000200 it would start to overwrite FWCONFIG data at 0x2ffc0000 with ID8  BL32,  OP-TEE extra 1, data

2. Why does OPTEE set a larger size in the header for BL32 extra 1 than available in SRAM for OT-TEE ?

3. and why does OPTEE ignore the CFG_TSZR_RAM size setting t(to reduce the size for SYSRAM) in the conf.mk file ?

4. Where does BL2 get the base address 0xde000000 and size from (see log below) ?

5. Is 0xde000000 the address BL2 will try to load image ID#9 (BL32 Extra 2) ?

6. What is/could be wrong ?

7. is there a "good boot" log of an DK or EV board using ECO 5.0.0 to see what the  memory locations are  used by BL2 for loading the FIP images ?

Boot log after manually changing the size to 0x10000 in the header:

INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.8-stm32mp1-r1.0(debug):()
NOTICE: BL2: Built : 15:24:01, Sep 11 2023
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
INFO: Memory size = 0x20000000 (512 MB)
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0x2ffff000
INFO: Image id=1 loaded: 0x2ffff000 - 0x2ffff1ea
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffc0000
INFO: Image id=4 loaded: 0x2ffc0000 - 0x2ffc002c
INFO: OPTEE ep=0x2ffc0000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x0
INFO: flags=0x0
INFO: nb_images=0x2
NOTICE: DEBUG: parse optee image #0
NOTICE: DEBUG: header->optee_image_list[num].image_id=0x0
NOTICE: DEBUG: OPTEE_PAGER_IMAGE_ID=0
NOTICE: DEBUG: OPTEE_PAGED_IMAGE_ID=1
NOTICE: DEBUG: init_load_addr=0x2ffc0200
NOTICE: DEBUG: init_size=0x10000
NOTICE: DEBUG: image_info->image_base=0x2ffc0000
NOTICE: DEBUG: image_info->image_max_size=0x22000
NOTICE: DEBUG: parse optee image #1
NOTICE: DEBUG: header->optee_image_list[num].image_id=0x1
NOTICE: DEBUG: OPTEE_PAGER_IMAGE_ID=0
NOTICE: DEBUG: OPTEE_PAGED_IMAGE_ID=1
NOTICE: DEBUG: parse_optee_image

NOTICE: DEBUG: init_load_addr=0xde000000
NOTICE: DEBUG: init_size=0x84000
NOTICE: DEBUG: image_info->image_base=0xde000000
NOTICE: DEBUG: image_info->image_max_size=0x2000000
INFO: BL2: Loading image id 8
INFO: Loading image id=8 at address 0x2ffc0200
WARNING: Image id=8 size out of bounds
ERROR: BL2: Failed to load image id 8 (-27)

 

This discussion is locked. Please start a new topic to ask your question.
14 REPLIES 14
debugging
Lead

Thank for the reply, but still wondering what are the key selection criteria to make a decision between OP-TEE in DDR or internal RAM ?

debugging
Lead

i assume this should be : this is not mandatory for every product  

It depends the use case, . In other words, if the product does need the protection of malicious attacks just use DRAM.

 

Product security is a big and complex subject really depending on the product. This needs to be global (HW + SW) and coherent from the production of the product and also after life of the product.

 

You can have an overview of the different tools available on STM32MP1 = https://wiki.st.com/stm32mpu/wiki/Security_overview

 

You may also request help from partners (like proven run).

 

After you decided which OP-TEE services are mandatory for your product, table https://wiki.st.com/stm32mpu/wiki/How_to_configure_OP-TEE#OP-TEE_core_configuration is here to advice between the 2 choices (internal or external RAM).

debugging
Lead

Thank for the feedback. Still stuck at the AXI 480 error. See my post. This happens  both  with OPTEE in DDR or in SRAM, I can switch between those quickly using custom build boot scripts. Both  results in same problem and it has taken me a month now to boot a simple board with discrete power and still unsuccessful. Spending many nights and days on this. I have no clues anymore. :slightly_frowning_face: