2022-10-19 9:48 AM
In engineering mode (BOOT0:off, BOOT2:On) I want to update my cortex-m4 firmware from CMD, not an IDE.
What is the command to do so?
Thank you!
Note: I tried using the STM32_Programmer_CLI executable but it keeps seeing the a7 only, I cant communicate with the m4.
Note: I think the IDE uses OpenOCD to do so but I can't find how to extract the command line it uses.
2022-10-25 1:36 AM
Hi @ufo2ofu
Engineering mode could only be used with debuggers using JTAG/SWD.
You could probably load Cortex-M4 FW using openOCD, but I have no information how to do it.
It would be much straightforward using CubeIDE (see example in https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-M4) or 3rd party IDE/debuggers (e.g. Keil, IAR, Lauterbach)
Please note that there is no embedded flash in STM32MP1 (FW is running from internal RAM only), so, in a running platform, the Cortex-M4 firmware is loaded from external Flash in SRAMs by uBoot or Linux (See https://wiki.st.com/stm32mpu/wiki/Boot_chain_overview#STM32MP15_boot_chain and https://wiki.st.com/stm32mpu/wiki/Linux_remoteproc_framework_overview#Remote_processor_boot).
Note that for STM32MP1 series, CubeProgrammer is only using USB (or UART) to connect to the platform and this is not available in Engineering mode (See https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP135x-DK/Let%27s_start/Populate_the_target_and_boot_the_image).
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.