2021-04-19 12:03 AM
Hello ,
I followed 1 qt-wpe-simple-browser
from here : https://wiki.st.com/stm32mpu/wiki/How_to_install_a_simple_web_browser
but getting the error in launching the browser on executing this command :
qt-wpe-simple-browser http://google.com
QQmlApplicationEngine failed to load components
qrc:/main.qml:3:1:module "org.wpewebkit.qtwpe" is not installed
which package i have to install?
I am already connecteed to network and I am on Ecosystem 3.0
regards,
D
Solved! Go to Solution.
2021-04-20 2:59 AM
Hello @darla14
Thank you very much for your feeback.
I take your questions as they come.
1/ The web browser can not connect to the google URL.
Could you check the board has an IP address. The commands
root@stm32mp1:~# ifconfig eth0or if you have a WIFI connection
root@stm32mp1:~# ifconfig wlan0should show the field inet addr with an IP address.
If not, please check your RJ45 connection or refer to the wiki pages related to the WIFI setup here or there.
If your board has an IP address, perhaps your board is behind a proxy. In such a case, export these two environment variables:
root@stm32mp1:~# export HTTP_PROXY="http://<your proxy url>:<port>"
root@stm32mp1:~# export HTTPS_PROXY="http://<your proxy url>:<port>"NB: there is no typo in the second expression: the URL is http and not https.
2/ The screen goes black after systemctl stop weston@root
That's the expected behaviour. With the qtwayland environment, you don't need to apply this command. I am sorry, I didn't see you were using only egls.
3/ ULR fetching error with apt-get install qtwayland
That may happen some time to time. I didn't succeed in identifying the underlying problem. However, it happens to be transient errors when I saw them (twice or three times since we put in production the OpenSTLinux repository). If these errors are not transient from your side, I would be glad if you could open a new topic related to these errors.
4/ Using qt-wpe-simple-browser with egls
By running the following commands:
root@stm32mp1:~# systemctl stop weston@root
root@stm32mp1:~# export QT_QPA_PLATFORM=eglfs
root@stm32mp1:~# export QML2_IMPORT_PATH='/usr/lib/qt5/qml/'
root@stm32mp1:~# export QT_QPA_EGLFS_ALWAYS_SET_MODE='1'
root@stm32mp1:~# qt-wpe-simple-browser http://google.comI am able to see the web browser on the screen of my stm32mp157f-dk2 board.
Best regards,
--JM
2021-04-19 12:06 AM
this looks like a Qt issue and Qt forum dwelings are more likely to answer your question
2021-04-19 2:55 AM
Hello @darla14
I think the wiki page is a bit misleading.
The error you get comes from the missing declaration:
root@stm32mp1:~# export QML2_IMPORT_PATH='/usr/lib/qt5/qml/'If the launch failed again, try to declare (assuming your in the qtwayland environment):
root@stm32mp1:~# export QT_QPA_PLATFORM=wayland-egl
root@stm32mp1:~# export QT_QPA_EGLFS_ALWAYS_SET_MODE="1"Tell me if this works. If so, I will get in touch with the wiki author to fix the web page when coming back from my holidays.
Best regards,
--JM
2021-04-19 4:08 AM
thanks, i was able to load it after exporting the path but unfortunately the webpage could not load the url
it shows :
Host www.google.com not found
Failed to load URL : http://WWW.GOOGLE.COM
I will test more.
STrange thing after executing systemctl stop weston@root , screen goes black . I had to connect to HDMI to see the page.
Dont we have to execute systemctl start weston@root at some point?
there are 3 steps
1> using Qt
2.Using Python
3> using eglfs or wayland.(whats teh difference)
I used eglfs because i get some url fetching error with apt-get install qtwayland (pointing some error in the url at 5.10.10 location.
I think 3rd Step is in addition and a pre-requisite with Step 1 OR 2 .It appeas from wiki that 1 OR 2 alone are sufficient.
Regards,
2021-04-20 2:59 AM
Hello @darla14
Thank you very much for your feeback.
I take your questions as they come.
1/ The web browser can not connect to the google URL.
Could you check the board has an IP address. The commands
root@stm32mp1:~# ifconfig eth0or if you have a WIFI connection
root@stm32mp1:~# ifconfig wlan0should show the field inet addr with an IP address.
If not, please check your RJ45 connection or refer to the wiki pages related to the WIFI setup here or there.
If your board has an IP address, perhaps your board is behind a proxy. In such a case, export these two environment variables:
root@stm32mp1:~# export HTTP_PROXY="http://<your proxy url>:<port>"
root@stm32mp1:~# export HTTPS_PROXY="http://<your proxy url>:<port>"NB: there is no typo in the second expression: the URL is http and not https.
2/ The screen goes black after systemctl stop weston@root
That's the expected behaviour. With the qtwayland environment, you don't need to apply this command. I am sorry, I didn't see you were using only egls.
3/ ULR fetching error with apt-get install qtwayland
That may happen some time to time. I didn't succeed in identifying the underlying problem. However, it happens to be transient errors when I saw them (twice or three times since we put in production the OpenSTLinux repository). If these errors are not transient from your side, I would be glad if you could open a new topic related to these errors.
4/ Using qt-wpe-simple-browser with egls
By running the following commands:
root@stm32mp1:~# systemctl stop weston@root
root@stm32mp1:~# export QT_QPA_PLATFORM=eglfs
root@stm32mp1:~# export QML2_IMPORT_PATH='/usr/lib/qt5/qml/'
root@stm32mp1:~# export QT_QPA_EGLFS_ALWAYS_SET_MODE='1'
root@stm32mp1:~# qt-wpe-simple-browser http://google.comI am able to see the web browser on the screen of my stm32mp157f-dk2 board.
Best regards,
--JM
2021-04-23 12:55 AM
thanks a lot ! worked for me as well.
i see we have used eglfs.
will try with wayland .
Tx,
Regards,
D
2021-04-26 1:41 AM
Hi @darla14
I am glad to see you fixed the issue.
Keep me posted with the wayland attempt if needed.
Best Regards.
--JM
"To help community to find solutions, please click on "Select as Best" for reply which solved your issue or answered your question."
2023-02-07 11:15 PM
@Jean-Marc B I've tried kirkstone branch and I cannot even build qt-wpe-simple-browser due cog build issue mentioned here: https://github.com/Igalia/meta-webkit/issues/446
Even when resolve it somehow starting browser just display white background but no webpage content is loaded. Did somebody check it on kirkstone branch? Thanks.
2023-02-08 4:20 AM
Hi @MBeli.1
As this post is two years old and successfully resolved, could you open a new one please?
Best regards,
--JM
2023-02-08 4:26 AM
@Jean-Marc B thanks for update. Added: https://community.st.com/s/question/0D53W0000274TnISAU/gcnanouserlandmultibinarystm32mp-issue-with-gbmh?t=1675858912318