2023-02-07 11:07 PM
We're are trying to use BKPSRAM in application code insecurely. According to the stm32mpu BKPSRAM_internal_memory page, we need to "set BKPSRAM as non-secure and degrade low power modes support, removing Standby mode"
Apart from setting the etzpc peripheral in the devicetree to non-secure [DECPROT(STM32MP1_ETZPC_BKPSRAM_ID, DECPROT_NS_RW, DECPROT_UNLOCK)]
what else is necessary in TF-A?
2023-02-07 11:52 PM
Hi @JRobi.3 ,
Take care of the warning banner :
"Default OpenSTLinux delivery prevents to define BKPSRAM as non-secure. This requires to modify TF-A source code with one of the following strategies:
This means removing STM32_PM_CSTOP_ALLOW_STANDBY_DDR_SR from the node below :
&pwr_regulators {
system_suspend_supported_soc_modes = <
STM32_PM_CSLEEP_RUN
STM32_PM_CSTOP_ALLOW_LP_STOP
STM32_PM_CSTOP_ALLOW_LPLV_STOP
STM32_PM_CSTOP_ALLOW_LPLV_STOP2
STM32_PM_CSTOP_ALLOW_STANDBY_DDR_SR
>;
system_off_soc_mode = <STM32_PM_SHUTDOWN>;
vdd-supply = <&vdd>;
vdd_3v3_usbfs-supply = <&vdd_usb>;
};And as said this can imply further modification in TF-A or OP-TEE source code. ( eg : some check of secure state of the BKPSRAM.
Olivier