cancel
Showing results for 
Search instead for 
Did you mean: 

Interfacing of Optical Ethernet Module with STM32MP257F-EV1

Amruta_Dixit
Associate II

The project requirement is to use optical ethernet with STM32MP257F. I want to try this interfacing first at STM32MP257F EV1 with some copper to optical Ethernet converter module, but in STM32MP257F EV1, Ethernet pins are not available for interfacing. Kindly suggest some solution for using optical ethernet with STM32MP257F.
     Kindly send the solution as early as possible.
     Thank you

 With Best Regards,
 Dr. Amruta S. Dixit

2 REPLIES 2
Gregory PLANCHON
ST Employee

Hi @Amruta_Dixit ,

 

Could you please explain why you need this setup?

I don't think it is possible on the STM32MP257F EV1 board, as it was not intended for this purpose.

 

Regards,

Grégory 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PatrickF
ST Employee

Hi @Amruta_Dixit 

On EV1 board, would be complex to un-solder components and adding wires to reconnect another RGMII device while maintaining signal/power integrity.

Might be possible for an ugly prototype, assuming it might not work or give stable behavior.

If you don't want to develop now your own board, maybe look to 3rd party SOM using STM32MP257 (Digi, Engicam, Kar-Ro, Phytec, Myir, PowerTip, BytesAtWork, Cargt, etc...). Those might have RGMII pins exposed to their boundaries.

 

Regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here